I want to boot from flash in S32R294 EVB.
But Boot Rom Code stops like below.
What should I do to issue this issue?
Starting reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&E\s32e200_s32r294.mac) ...
REM This script is compatible with S32R294 devices.
REM Clean GPRs to remove residual data after using algorithm
REM Initialize all of the Main DSRAM - 1024KB
Initializing RAM from $40000000 to $400FFFFF.
Initializing Ram Block 0x40000000-0x400FFFFF.
Reset script (C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\win32\gdi\P&E\s32e200_s32r294.mac) completed.
Running Boot Rom ...
Initializing Ram Block 0x40000000-0x4000000F.
Stopping Boot Rom code. (Did not exit boot rom as expected)
Boot Rom execution stopped. (pc=0x00002048)
S32R294 Device detected
BRs.
Hyunung Park
Hi, @HyunungPark ,
Very sorry for checking this case very late.
Please let us know if you were able to resolve the issue, if yes what was the problem.
Thank you. Best regards.
-Mehul Patel