BCC_S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BCC_S32K144

1,914件の閲覧回数
rajesh1
Contributor I

When i am importing BCC(battery cell controller) example in s32 design studio it showing  messege: kinetis 

SDK SDK_s32k1xx_15 is not installed. screenshot is attached in attachment.can u help me out to install 

kinetis SDK SDK_s32k1xx_15.

タグ(3)
0 件の賞賛
5 返答(返信)

1,744件の閲覧回数
rajesh1
Contributor I

how to install this??

0 件の賞賛

1,744件の閲覧回数
raresvasile
NXP Employee
NXP Employee

Hi,

Please install RTM 3.0.0 from: https://www.nxp.com/lgfiles/updates/S32DS/S32DS_ARM_v2018.R1_UP9.zip 

Thank you,

Rares

0 件の賞賛

1,626件の閲覧回数
Kallappa
Contributor III

Hello,


I am also facing the same issue regarding the kinetes SDK . as you suggested I downloaded the SDK but not be able to include or add to the S32DS so it will really helpful if you help here.

Thanks in Advance.

0 件の賞賛

1,614件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is your S32DS Version? 

 

Jiri

0 件の賞賛

953件の閲覧回数
Zyuan17
Contributor III
Hi, I encountered the same problem. Do you have a direct download link to the SDK_s32k1xx_15? I am currently using S32K142+MC33771C.
0 件の賞賛