S32K SDK Example - Function call on configurable period using LPIT timer.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K SDK Example - Function call on configurable period using LPIT timer.

S32K SDK Example - Function call on configurable period using LPIT timer.

* Brief Periodical function call by LPIT timer
********************************************************************************
* Detailed Description:
* Application performs function call on configurable period. Period in ms is
* taken from potentiometer connected to ADC.
*
*
*
* ------------------------------------------------------------------------------
* Test HW: S32K144EVB,
* MCU: S32K144
*
* Debugger: PeMicro USB-ML-PPCNEXUS
*
* Target: internal_FLASH (debug mode, debug_ram and release mode)
*

标签 (2)
附件
无评分
版本历史
最后更新:
‎02-17-2017 02:29 AM
更新人: