Where could find demo code based on single-shunt for S12ZVM-EFP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where could find demo code based on single-shunt for S12ZVM-EFP?

2,250 Views
peter_shi
Contributor II

There are three current sampling methods whichusesshunts in inverter legs as current sensors,tri-shunt,dual-shuntandsingle-shunt. S12ZVM-EFP supportsdual-shunt and single-shunt.
There are two demo projects, one is for dual-shunt and another one is for single-shunt.

0 Kudos
Reply
4 Replies

1,940 Views
sunkemiao2021
Contributor I

above address which aboat  download the code AN5327SW is error.I can not open it.Who can tell me the right address. thanks

0 Kudos
Reply

2,144 Views
peter_shi
Contributor II

EFP demo code has improved the startup performance as below based on dual shut sampling. AN5327 is an old software. Did you have single shut sampling for good startup performance?

Dedicated optimized for fuel pump application to achieve robust and fast start up. It meets the
strict start up condition < 150 ms from standstill to the rated speed

0 Kudos
Reply

2,144 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The SW for the AN5327 which is mentioned on the S12ZVM-EFP site https://www.nxp.com/design/development-boards/automotive-motor-control-development-solutions/magniv-...  

can be downloaded from this link:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN5327SW.zip 

However, I would like to mention that this SW is for the MTRCKTSPNZVM128|Development Kit S12 MagniV | NXP 

 I hope it helps.

Best regards,

Diana

0 Kudos
Reply