What is the difference between S12X and S12Z core ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between S12X and S12Z core ?

991件の閲覧回数
ameykhatavkar
Contributor III

I wanted to know the difference between the S12X and S12Z core. If the things are implemented in the MCS12XDP512 can directly compatible with MC9S12ZVM.

Is there things that to be needs to be taken care before porting. Iam going through the stuffs available on this but I need immediate inputs on this.

ラベル(1)
0 件の賞賛
1 返信

507件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Amey,

Please look at my answer here:

https://community.freescale.com/message/604458#604458

I would like to add two more specific points:

1. S12Z MCUs have implemented ECC on RAM and Flash (you cannot use cumulative write into Flash).

2. Double bit ECC error, illegal opcode and illegal address access will cause Machine exception interrupt.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛