S9S12ZVLS3F0VFMR and S9S12ZVLS3AVFMR Distinction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S9S12ZVLS3F0VFMR and S9S12ZVLS3AVFMR Distinction

813件の閲覧回数
caesar_song
Contributor III

Dear All

    Woudly you kindly help to provide the  document of S9S12ZVLS3F0VFMR and S9S12ZVLS3AVFMR  different ,and the wafer lab explain,thanks.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

718件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 

S9S12ZVLS3 F0 V F MR   

S9S12ZVLS3 A  V F MR 

 

The F0 means mask set as well as letter A. There were two mask set with different number but the same and the difference was only manufacturing factory.

Because of this, NXP stopped distinguishing the part number in terms of place of manufacture and a new mask set label was invented ... “A”.

So mask set A is absolutely the same as mask set F0 which means mask 0N22G and corresponding errata list.

 

PCN 202103038F01  … Issue Date: Apr 17, 2021  Effective Date: Jul 16, 2021 

Attached is a file from PCN which explains numbering (I explained above) at slide 5.

 

Best regards,

Ladislav

0 件の賞賛
返信

802件の閲覧回数
caesar_song
Contributor III

The PCN for S9S12ZVLS3F0VFMR and S9S12ZVLS3AVFMR 

0 件の賞賛
返信

803件の閲覧回数
caesar_song
Contributor III

Would you  help to provide the PCN for S9S12ZVLS3F0VFMR to S9S12ZVLS3AVFMR,thanks 

0 件の賞賛
返信