Hello All,
I am using Codewarrior v 5.7.0 and am working on an application that requires an RTI to update graphics to an LCD. I have scanned the forums throughly and came up with this scheme for my RTI. I am using the 9S12XDP512 on an ADAPT9S12XD board over a serial RS232 connection.
#include <hidef.h> /* common defines and macros */#include <mc9s12xdp512.h> /* derivative information */#pragma LINK_INFO DERIVATIVE "mc9s12xdp512"#pragma CODE_SEG __NEAR_SEG NON_BANKEDinterrupt void RTI_ISR(void) { PTP = 0x80; //turns on an onboard LED CRGFLG = 0x80;}#pragma CODE_SEG DEFAULTvoid RTIinit(void) { RTICTL = 0x63; CRGINT = 0x80; CRGFLG = 0x80;}void main(void) { DDRP = 0xFF; //Set Port P to Output RTIinit(); EnableInterrupts; for(;;) {} /* wait forever */}
VECTOR ADDRESS 0xFFF0 RTI_ISR //in my .prm file
This code is not turning on the LED as expected meaning it never enters the ISR. Any help or suggestions would be greatly appreciated. Thanks!
Hello
I tested this code on my CodeWarrior HC12 V5.1 (The current release for HCS12X).
I set a breakpoint at the beginning of the function RTI_ISR and the interrupt is generated.
Did you try setting a BP in the interrupt? Is application stopping?
CrasyCat
Thanks for the reply. I did attempt a BP at the ISR and it appears to stop the application from running when it enters the ISR. Any code attempted after initializing the RTI does not run and I lose connection to the 9S12X. Is this a possible issue with the placement of my code (_Startup is at $B100)?
Hello Kef,
I am using a banked memory model. The code originally had a startup at $C000, but code would not run at that place (application failed) so I moved it in order for it to work (I see now that was wrong). I have only began to run into problems implementing interrupts, as before I was using SCI, ATD etc with no issues. This is my first experience with banked memory model as previously I have only used the HC12B32. Where should my _Startup be initialized and do I need to manipulate GPAGE and/or PPAGE? Thank you so much
I have created a fresh project file with the prm (untouched except for the interrupt vector) having nonbanked ROM enter at $C000. This only code I am running is the original interrupt scheme seen above. The application does not run when I use $C000 as the _Startup address. I have even tried simply turning on a pin with no interrupt to no avail. I am using the ubug12x program to connect serially to my uC board and giving the command GO $C000. Am I using the banked memory incorrectly to run programs? I apologize for my lack of familiarity with this uC. Thanks in advance.
Is program really loaded to target MCU using ubug12x? BTW is it BDM pod?
If you load program "serially", then as I understand it, there is some program running on target MCU, which accepts program sent over SCI and writes it to flash. If it is so, then there must be some restrictions and requirements for where and how should you place and specify your interrupt vectors. For example your ubug stuf may require initializing some jump table in RAM. Check the docs. Anyway 0xC000 address should be perfectl for _Startup routine.