PE Bean for 80-pin MC9S12DG256?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE Bean for 80-pin MC9S12DG256?

4,082 Views
TheBroadLea
Contributor I
Our application uses an 80-pin MC9S12DG256, but I only find a 112-pin bean.  I am using CodeWarrior for HC12 v4.5 and Processor Expert v2.96.  I don't see any updates at processorexpert.com.  Is there perhaps a substitute bean that I should use?
Labels (1)
0 Kudos
Reply
3 Replies

658 Views
EMontanez
NXP Employee
NXP Employee
Processor Expert support for the 80 pin package is scheduled for releaset in the fall. For now, I would suggest using the 112-pin. The modules are the same, just be aware of the pin changes from your hardware implementation.
0 Kudos
Reply

658 Views
mke_et
Contributor IV
I'm not sure it would apply for your case, but you may have to set some 'default conditions' for the 80-pin part to keep power consumption to a minimum that could be different than for the full pinned part. 
0 Kudos
Reply

658 Views
TheBroadLea
Contributor I
Well, as it happens, there is a bean for an 80-pin DJ256, and that seems to be working fine so far.  Maybe that will get us by until the updates come out.
 
Thanks for the info.
0 Kudos
Reply