I am using MM9Z1J638 MCU, but there is a fast chip seems to be debugged by me, under the same environment another development board can enter debugging, but this one can not, how to unlock the chip?(cw 10.7)
The following is the error promotion
Conficm
Device is secure. Erase to unsecure?
No
Yes
"Launchinq xxx FLASH PnEU-MultiLink'has
encountered a problem. Wouild you like to
export diagnosticinformation and send it to
Freescale?
Error launchinq E245 FLASH PnE U-MultiLink
The target MCUis notresponding
Please turn MCU power off (Under 0.1v,
turn MCU power on, and then clickOK.
This will attempt to enter debug mode
througha power on reset sequenCe.
I just ran across this. I am assuming that you have RESETA and RESET tied together. Please note that flashing problems can occur when these pins are connected. A simple solution is to provide a 470nF capacitor at these reset pins to ground. This should allow you to program.
Regards,
Peter