MM9Z1_638 Power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1_638 Power consumption

ソリューションへジャンプ
1,730件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi there,

 

I´m using a MM9Z1_938 and I need to reduce the power consumption because I want to reduce the self heating of the IC. Is there a possibly or configuration to reduce the power consumption of the IC?

 

Regards

0 件の賞賛
1 解決策
1,659件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Boris_Bloxsberg,

Using the lower-power modes of the device.

Disabling unused peripherals:

danielmartynek_0-1637053944845.png

Make sure no inputs are floating, especially in the low-power modes.

 

Regards,

Daniel

元の投稿で解決策を見る

3 返答(返信)
1,717件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Boris,

The power consumption is proportional to the system clock frequency.

You need to reduce the frequency as much as possible for this application.

 

BR, Daniel

1,668件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

 

thanks for the reply. The clock frequency way is working.

Are there any other ways aviable?

 

regards

0 件の賞賛
1,660件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Boris_Bloxsberg,

Using the lower-power modes of the device.

Disabling unused peripherals:

danielmartynek_0-1637053944845.png

Make sure no inputs are floating, especially in the low-power modes.

 

Regards,

Daniel