Hi,
I´ve got a question regarding the absolute rating of the ISENSE - Pins. What is the maximum voltage at these pins?
I`ve got some issues with this pins. If I simulate a failure and apply 24V a this pin, I got a short circuit.
Does anybody know these problem? Or is there an additional config bit to prevent this short circuit?
regards
Solved! Go to Solution.
Hi,
The maximum rating is specified in Table 4:
And these are the conditions required for the ISENSEH and ISENSEL terminals (= pins). Line 1-3 Vinc (V in common) are for the ISENSEH to GND voltage and the ISENSEL to GND voltage. Line 4 Vind (V in differential) are for ISENSEH to ISENSEL voltage.
Best regards,
Tomas
Hi,
The maximum rating is specified in Table 4:
And these are the conditions required for the ISENSEH and ISENSEL terminals (= pins). Line 1-3 Vinc (V in common) are for the ISENSEH to GND voltage and the ISENSEL to GND voltage. Line 4 Vind (V in differential) are for ISENSEH to ISENSEL voltage.
Best regards,
Tomas