MM9Z1_638 ISENSE max. voltage rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1_638 ISENSE max. voltage rating

Jump to solution
1,180 Views
Boris_Bloxsberg
Contributor III

Hi,

I´ve got a question regarding the absolute rating of the ISENSE - Pins. What is the maximum voltage at these pins?

I`ve got some issues with this pins. If I simulate a failure and apply 24V a this pin, I got a short circuit.

Does anybody know these problem? Or is there an additional config bit to prevent this short circuit?

regards

0 Kudos
1 Solution
1,174 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The maximum rating is specified in Table 4:

Table 4.JPG

And these are the conditions required for the ISENSEH and ISENSEL terminals (= pins). Line 1-3 Vinc (V in common) are for the ISENSEH to GND voltage and the ISENSEL to GND voltage. Line 4 Vind (V in differential) are for ISENSEH to ISENSEL voltage.

Isense.JPG

Pic.png

Best regards,

Tomas

View solution in original post

1 Reply
1,175 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The maximum rating is specified in Table 4:

Table 4.JPG

And these are the conditions required for the ISENSEH and ISENSEL terminals (= pins). Line 1-3 Vinc (V in common) are for the ISENSEH to GND voltage and the ISENSEL to GND voltage. Line 4 Vind (V in differential) are for ISENSEH to ISENSEL voltage.

Isense.JPG

Pic.png

Best regards,

Tomas