MCU Flasher for MM9z1_638

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU Flasher for MM9z1_638

ソリューションへジャンプ
811件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,


I want to implement an own software applicantion to flash the MM9z1_638. Could somebody recommand a device to flash this type of MCU and this type of usecase?



Thanks.

0 件の賞賛
返信
1 解決策
775件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

There is no such list.

PEMicro programmers are recommended on each NXP S12Z MCU website though.

S12ZVM:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

 

BR, Daniel

元の投稿で解決策を見る

3 返答(返信)
787件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Boris_Bloxsberg,

Do you mean a debugger/programmer?

Since the MM9Z1_638 has the S12Z core, you can use those that support S12Z (MagniV).

For example PE Micro Multilink:

https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=3

danielmartynek_0-1689148077888.png

 

Regards,

Daniel

782件の閲覧回数
Boris_Bloxsberg
Contributor III

Thanks @danielmartynek  for the reply.

Yes, I need a programmer. Is there a list aviable with supported programmers for the S12Z? 

Regards,

 

0 件の賞賛
返信
776件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

There is no such list.

PEMicro programmers are recommended on each NXP S12Z MCU website though.

S12ZVM:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

 

BR, Daniel