MC9S12XEP100这款MCU有关3.3V供电问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12XEP100这款MCU有关3.3V供电问题

613件の閲覧回数
kangjunyan
Contributor I

你好: 请问MC9S12XEP100这款MCU,PDF文档上显示的供电电压范围在3.15V-5.5V,我用3.3V供电,系统的电压如果在3.1V左右,这个MCU会不会死机。我用的复位电路芯片只要低于3.08V,复位芯片就会起作用,使MCU复位,但是这个MCU电压供电范围只在3.15V到5.5V,所以万一电压只有在3.12或者3.13V左右还没到复位芯片工作电压,MCU就不工作了,会出现什么样的情况?谢谢

0 件の賞賛
返信
2 返答(返信)

528件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

VLVRXA is defined to be 3.02V typically. It minimum value is guaranteed to be 2.97V

Below the 3.02V (the voltage drops down) the MCU resets and will keep in the reset up to deassert level VLVRXD=3.13V.

Best regards,

Ladislav

0 件の賞賛
返信

528件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Translated by translator: Hello: Will MC9S12XEP100 this MCU, PDF document shows the supply voltage range of 3.15V-5.5V, I use 3.3V power supply, the system voltage if the 3.1V or so, the MCU will not crash. I use the reset circuit chip as long as less than 3.08V, reset the chip will work, so that MCU reset, but the MCU voltage supply range only 3.15V to 5.5V, so if the voltage is only 3.12 or 3.13V or so To reset the chip operating voltage, MCU does not work, what will happen? Thank you

0 件の賞賛
返信