Is there any example about S12ZVML31_BLDC with Sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any example about S12ZVML31_BLDC with Sensor?

677 Views
w_lingjun
Contributor III

Hi,

I'm studying on the S12ZVM32EVB, and the motor can work using the attachment of AN5176 which is sensorless.

I want to use sensor to get the location, so I try to use the attachment of AN4718 with hall sensor. I do following two things:

1) Use the AN4718 project and modify file S12zvm.prm to fit for S12ZVML31, sensorless and with sensor both can't work. Is there any other places should I modify?

2) Use the AN5176 project and modify file MC9S12ZVML31_BLDC_Sensorless.c based on MC9S12ZVML128_BLDC.c, sensorless and with sensor both can't work. 

I compare file MC9S12ZVML128_BLDC.c of AN4718 and file MC9S12ZVML31_BLDC_Sensorless.c of AN5176, the timer channel assignment are different, HV_init() and LIN_init() used in AN5176, and APP improvement in AN4718, it seems that there is not any difference between them. Is there any important things I miss? Or there is any example about S12ZVML31_BLDC with Sensor? Thank you very much.

 

Best regards,

Sarah

0 Kudos
1 Reply

614 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Sarah,

AN5176 is about Using the High Voltage Physical Layer.

https://www.nxp.com/docs/en/application-note/AN5176.pdf 

Anyway, there is no Hall sensor BLDC demo ported on S12ZVML31.

But there is this migration guide that lists the differences between S12ZVM differences:

Migration Guide for S12ZVM Devices

Regards,

Daniel

0 Kudos