Hello,
I have a problem with the printf fonction.
I'm sorry for my bad english
My program is :
#include <hidef.h>
#include "derivative"
#include <stdio.h>
#include <termio.h>
int x=0;
int main(void)
{
{
if(x<20)
{
printf("%d\n",x);
x++;
return 0;
}
}
}
///////////////////////////////////////////////////////////////////////////////////////////
On HyperTerminal, I don't receive the printf.
I believe that my program is in the loop "while (!(SCI.SCxSR1 & 0x80) ) {};" in the termio.c. WHY ???
By default, what is the port used, SCI0 or SCI1 ?
How do I configure the connection in hyperterminal, knowing that I have a MC9S12DG128 ?
Best Regards
Julien
解決済! 解決策の投稿を見る。
The termio.c contains a routine TERMIO_Init for the setup, it might need to be adapted for the hardware.
Alternatively Processor Expert (or Device Initialization) can be used to setup the sci module.
Daniel
I don't see any harware initialization: somewhere in your code should be a line like:
Initialize_SCI();
.. or something similar, possibly including a baud-rate setting, parity-type, etc
Look into demo code for your CPU
The termio.c contains a routine TERMIO_Init for the setup, it might need to be adapted for the hardware.
Alternatively Processor Expert (or Device Initialization) can be used to setup the sci module.
Daniel
thank you for your answer, it's OK for the printf.
The baud rate was bad in TERMIO_Init().
Best Regards
Julien