How to realize PMSM high load low speed start

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to realize PMSM high load low speed start

742件の閲覧回数
maxxu
Contributor IV

Hi NXPtechnical team

      I refer to the FOC control application of s912zvm(AN5135). The official scheme, rotor position / speed estimation uses BEMF observer. This principle has requirements on the speed, which is not applicable to the occasion of starting at very low speed with large load.

      I need to be able to use the zero speed control scheme, whether the high-frequency injection method is used, and if the resources of s912zvm cannot be met, Can it be implemented on s32k series chips? I look forward to NXP's application in this regard.

                                                                   Thank you

0 件の賞賛
0 返答(返信)