High Freq MUX control (MC9S12XEP100)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

High Freq MUX control (MC9S12XEP100)

1,840件の閲覧回数
ernestsnaith
Contributor I
I need to serially output data at a rate of 3.125 MHz. The CPU is unable to meet the 3.125 MHz requirement after necessary logical operations are performed. Consequently I intend to multiplex a port and divide the output rate down by a factor of 8. The problem i currently have is how to drive the multiplexors 3 channel select pins. I would like to have three outputs from the microcontroller toggling at 3.125 MHz, 1.56 MHz and 0.78 MHz. However it would be required to align the 3 signals at the start of a byte transmission.
 
With the exception of alignment, is there a way of getting the microcontroller to do this with little software intervention? I cant see a complete solution using any of the following modules.
 
PWM - Although the signals could be produced i see no way of aligning channels.
ECT - Any solutions i have thought of require an interrupt for which i do not have the CPU time.
PIT - Ideal but can it toggle output pins?
 
Is there any way of solving this problem without additional circuitry?
 
Many Thanks
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

572件の閲覧回数
ernestsnaith
Contributor I
Good point, i had considered SCI but didnt think to look at SPI. Cheers
0 件の賞賛
返信

572件の閲覧回数
HSW
NXP Employee
NXP Employee
Why don't you just use one of the 3 SPIs to stream out your serial data?
0 件の賞賛
返信