ESD testing failure for MC9S12XET256MAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ESD testing failure for MC9S12XET256MAG

1,020 Views
kumara
Contributor I

we are using the controller MC9S12XET256MAG for our transmission ECU. While doing ESD test(Air discharge) near controller area, the controller is getting halt during the exposure.It's recovering only after the hard reset of the device. Kindly suggest some solution to rectify the same.

Tags (1)
0 Kudos
Reply
2 Replies

888 Views
chithanhhoang
Contributor II

I have the same problem on the LS1043A chip, my work around is to program the hw watchdog to reset if the cores are frozen because of ESD.

Not the ideal solution but work for me.

Hope my comment helps you.

0 Kudos
Reply

952 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

standard procedure.....

1) Could you please send a readable schematic of the MCU environment?

2) Also good to see whether PCB is OK especially all unused pins correctly (https://www.nxp.com/docs/en/application-note/AN3262.pdf ), no wire or plane under oscillator circuitry, correctly calculated load capacitances,.....

Best regards,

Ladislav

0 Kudos
Reply