Hello All,
I am studying on MM9Z1J638 intelligent battery sensor. I see that ADC results of voltage difference within each cell is kept in mV as well among with adc values (called raw values in demo code). I did not quite get how ADC result (raw values) are converted into miliVolts.
Given:
const u8 Vres [V_MAX_CHANNELS] = {VS_RES_0mV25, VS_RES_0mV25, VS_RES_0mV5, VS_RES_1mV};
Following shows this conversion:
Vsense[u8VChIdx].u16Raw = u16VsenseValue;
Vsense[u8VChIdx].u16mV = u16VsenseValue >> Vsense[u8VChIdx].u8Res;
Looking forward to see your comments.
Best
Kadir
解決済! 解決策の投稿を見る。
The resolution of the VSENSE channels is
To scale the result a divide by 1 / 2 / 4 / 4 can be used (or a shift >> 0 / 1 / 2 / 2 as in the code above).
The resolution of the VSENSE channels is
To scale the result a divide by 1 / 2 / 4 / 4 can be used (or a shift >> 0 / 1 / 2 / 2 as in the code above).
Hello again,
A question occured in my mind. I know that we have only one channel for voltage measurement. Why do we have different resolutions for each Vsense(x)?
Thanks in advance
Kadir,
the MM9Z1_638 is optimized to address 12V lead acid battery BMS systems but not limited to that. For the 12V system a single measurment channel would be enought (typically VSENSE2 - can measure 0..28V). For other applications, e.g. 24V systems two VSENSEx (VSENSE2 and VSENSE3) could be used. For e.g. 4 cell LiIon you would want 4 VSENSEx inputs.
The 4 VSENSEx inputs (ranges and resolutions) were selected as "trade-off" to adress different applications.
W.
Ok, I see now. For my application I utilized 4 channels of Vsense and the resoulutions are different. I also checked the manual. Thank you for your fast response.
Best
Kadir
Hello Wolfgang,
Thank you for your response. It solved my problem.
Have a good day
Kadir