Hello,
Thank you.
One value is missing in the "Real Time Data" in the Cal.c file.
Also, the array below is filled with 25 numbers, but your size is uint16_t lockupMap[2][12]; in the Cal.h
{1,10,20,30,40,50,60,70,80,90,100,110,120,
200,300,400,500,600,700,800,900,1000,1100,1200,1300}, // LockupMap
I believe it helps.
Best regards,
Diana