Hi all,
For days i've been trying to print something on my monitor, but without succes.
I use the MC9S12DP512 (CardHCS12) which has the Twinpeeks monitor on it. Thereby I use the OC-console and CodeWarrior.
The following example works in the Simulator and I can load it into the HCS12 with OC-console (after using sreccvt and updating the .prm-file to prevent "invalid bank load address errors" ).
When I run the prog, the HCS12 responds (I assume, because the default led stops) but doesn't show anyting on the OC-console.
#include "Cpu.h"
#include "PE_Types.h"
#include "PE_Error.h"
#include "PE_Const.h"
#include "IO_Map.h"
#include <stdio.h>
#include <termio.h>
void main(void)
{
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
PE_low_level_init();
/*** End of Processor Expert internal initialization. ***/
TERMIO_Init();
for (; {
(void)printf("Hello %s\n", "World");
}
/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
for(;{}
(I also tried the Guess the Number-tutorial without succes)
Can somebody give me a hint how to get printf working??
Thank a lot,
Sander Dijkstra