9S12XEG384 bank F9 is not programmed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12XEG384 bank F9 is not programmed

ソリューションへジャンプ
807件の閲覧回数
leroy_o
Contributor III

I have a problem with the flashing of the F9 flash memory bank after having switched a project from 9S12XEG128 to 9S12EG384 recently.

 

The F9 flash memory bank is declared in the prm project file, also, F9 memory locations appear in the project.abs.s19 file, but this code is not programmed in actual flash memory.

 

I use a Freescale PE USB multilink interface to perform the actual flashing, it worked with the 9S12XEG128, but after flashing, object code in the F9 bank appear as "FFFFFFFFFFFFFFFF...".

 

Has someone encoutered the same kind of problem and solved it?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
657件の閲覧回数
leroy_o
Contributor III

I solved the problem:

I forgot to also perform in HCS12MultilinkCyclone Pro:

- Select derivative

    - MC9S12XEQ384


Problem solved.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
658件の閲覧回数
leroy_o
Contributor III

I solved the problem:

I forgot to also perform in HCS12MultilinkCyclone Pro:

- Select derivative

    - MC9S12XEQ384


Problem solved.

0 件の賞賛
返信