Document about GAP and GATT BLE for Rapid IOT ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Document about GAP and GATT BLE for Rapid IOT ?

1,160件の閲覧回数
wichaitossamart
Contributor I

 Hi,

Are there any document about GAP and GATT BLE on Rapid IOT for sensors ? I would like to connect Rapid IOT from ESP32.

Thank you

ラベル(1)
4 返答(返信)

877件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Do you mean something like this? 

Creating a custom profile using NXP BLE stack – Server  

How to create a Custom Profile - Client 

 

If you look for further information regarding the BLE transmission protocol, I believe this link will also be helpful which it's some of the information available in the NXP knowledge-center.

Besides that, you can also check the Bluetooth® Low Energy Applications Developer’s Guide and the Bluetooth Low Energy API reference manual

Best regards, 

Estephania 

877件の閲覧回数
yoursunny
Contributor III

These document seems to be targeting the KW41 chip. However, there isn't any SDK examples for the KW41 ("import SDK examples" shows an empty list after selecting KW41).

I want to create GATT characteristics to report sensor readings.

How can I use BLE from K64 chip, with the factory KW41 firmware? Or, if I have to program the KW41, is there a "hello_world" for me to get started?

0 件の賞賛

877件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

There is a project for KW41Z but not as "Example project", you have to import it from the file system, it is located under SDK path at SDK_2.2_RapidIoT_MKW41Z4\boards\rpk_kw41z\rapid_iot_apps\rpk_kw41z_hybrid

This is the default application flashed in KW41Z

0 件の賞賛

877件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

As the KW41Z it's  running a host controlled interface you could send the commands to work with the network, I believe there are quite useful posts and examples in the community such as these: 

IDE 

https://community.nxp.com/thread/490773 

If you still have any doubt after reading those, just let me know. 

Regards, 

Estephania

0 件の賞賛