I've noticed that for my P2041, the ENTRY_SIZE for the spin table is 32 but the T1040 and the T2080, the ENTRY_SIZE is 64. Why is there a difference? And to release a core, I need to specify R3 and R6. What should be specified for R3 and R6? Thanks!
The T1040 and the T2080 have 64-bit ISA Power Architecture processor cores. The P2041 has e500mc core which is a 32-bit implementation of the Power ISA.