Hello everybody,
Does someone of you already manage to get a 10gigabit connection through the ethernet copper interface with the p4080ds?
Even with the freescale SDK, I can not establish a connection between my p4080 board and a dedicated computer with an ethernet card and a linux.
I know my question is very large but I can enter more in the details if someone of you works on this specific subject.
I already work on the SERDES errata 8, changing the hwconfig and trying several RCW without success.
I dream of the day during which I will get a ping...
Any suggestion on how to process is greatly appreciated!
Simon
I just spoke to one of our team members in a test lab. They have verified 10g copper working on their setup. I asked them to give me the u-boot log and hwconfig variable. The u-boot is an internal build likely based off SDK 1.2. The important thing is to note the rcw and hwconfig settings.
Also, what slot is the 10g XAUI riser connected to? Slot 5 corresponds to FM1@TGEC1 and Slot 4 corresponds to FM2@TGEC1.
I recommend trying to ping directly from u-boot before loading Linux. It can help narrow down where the problem occurs.
-----
U-Boot 2011.06-rc2-00009-g719876a-dirty (May 18 2012 - 13:45:22)
CPU0: P4080E, Version: 2.0, (0x82080020)
Core: E500MC, Version: 2.0, (0x80230020)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
PME: 399.996 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e18181e 0000cccc
00000010: 38424400 3c3c2000 fe800000 61000000
00000020: 00000000 00000000 00000000 008b0000
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM EBJ21EE8BAFA-DJ-E
Detected UDIMM EBJ21EE8BAFA-DJ-E
CS2 is disabled.
CS3 is disabled.
Address hashing enabled.
CS2 is disabled.
CS3 is disabled.
Address hashing enabled.
2 GiB left unmapped
DDR: 4 GiB (DDR3, 64-bit, CL=9, ECC on)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 2048 KB enabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_ESDHC: 0
EEPROM: Invalid ID (ff ff ff ff)
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: Root Complex, no link, regs @ 0xfe201000
PCIe2: Bus 01 - 01
PCIe3: Root Complex, no link, regs @ 0xfe202000
PCIe3: Bus 02 - 02
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 101.8.0
FM1@DTSEC2 connected to Vitesse VSC8244
FM1@TGEC1 connected to Teranetics TN2020
Fman2: Uploading microcode version 101.8.0
FM2@DTSEC3 connected to Vitesse VSC8234
FM2@DTSEC4 connected to Vitesse VSC8234
FM2@TGEC1 connected to Teranetics TN2020
FM1@DTSEC2, FM1@TGEC1, FM2@DTSEC3, FM2@DTSEC4, FM2@TGEC1
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1,addr_hash=true
Hi All,
I'm working with 2- p4080ds systems, both systems are identical. below is my u-boot env.
U-Boot 2010.12-00007-g4114d25 (Jan 26 2011 - 22:35:21)
CPU0: P4080E, Version: 2.0, (0x82080020)
Core: E500MC, Version: 2.0, (0x80230020)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz, CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz, CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999 MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
PME: 399.996 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e1e181e 0000cccc
00000010: 40464000 3c3c2000 fe800000 61000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
DRAM: Initializing....using SPD
Detected UDIMM(s)
Detected UDIMM(s)
CS2 is disabled.
CS3 is disabled.
CS2 is disabled.
CS3 is disabled.
2 GiB left unmapped
DDR: 4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
FLASH: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 2048 KB enabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_ESDHC: 0
EEPROM: NXID v0
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1, regs @ 0xfe202000
02:00.0 - 1095:3132 - Mass storage controller
PCIe3: Bus 01 - 02
Video: No radeon video card found!
In: serial
Out: serial
Err: serial
Net: Fman: Uploading microcode version 101.8.0.
Dtsec: PHY is Vitesse VSC8244 (fc6c2)
Fman: Uploading microcode version 101.8.0.
Dtsec: PHY is Vitesse VSC8234 (fc623)
Dtsec: PHY is Vitesse VSC8234 (fc623)
Dtsec: PHY is Vitesse VSC8234 (fc623)
Dtsec: PHY is Vitesse VSC8234 (fc623)
FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4, FM2@TGEC1
Hit any key to stop autoboot: 0
=> printenv
baudrate=115200
bdev=sda3
bootargs=console=ttyS0,115200 ip=10.137.108.232:10.137.108.165:10.137.108.129:255.255.255.128::eth0:none root=/dev/nfs rw nfsroot=10.137.10
8.165:/tftpboot/loads/board1/rootfs
bootcmd=tftp $loadaddr $bootfile; tftp $fdtaddr $fdtfile; bootm $loadaddr - $fdtaddr
bootdelay=5
bootfile=board1/fsl_p4080-uImage-WR4.3.0.0_cgl
c=ffe
consoledev=ttyS0
dir=b25229/01-20
eth=FM1@DTSEC2
eth1addr=00:04:9F:02:21:2E
eth2addr=00:04:9F:02:21:2F
eth3addr=00:04:9F:02:21:30
eth4addr=00:04:9F:02:21:31
eth5addr=00:04:9F:02:21:32
eth6addr=00:04:9F:02:21:33
eth7addr=00:04:9F:02:21:34
eth8addr=00:04:9F:02:21:35
eth9addr=00:04:9F:02:21:36
ethact=FM1@DTSEC2
ethaddr=00:04:9F:02:21:2D
fdtaddr=c00000
fdtfile=board1/p4080ds_36b.dtb
fileaddr=1000000
filesize=3DECE9
fman_ucode=0xFEF000000ULL
gatewayip=10.137.108.129
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1,ecc=off
ipaddr=10.137.108.232
loadaddr=1000000
netdev=eth0
netmask=255.255.255.128
rootpath=/tftpboot/loads/board1/rootfs
serverip=10.137.108.165
stderr=serial
stdin=serial
stdout=serial
uboot=u-boot.bin
ubootaddr=0xeff80000
Environment size: 1182/8188 bytes
After changing hwconfig to "fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1,ecc=off", (serdes config to make bank2/3 power-on). I started seeing 10g card in slot4 FM2@TGEC1.
for testing purpose I connected both 10g to local lan, keeping rest of the interfaces disconnected. (not trying to boot from 10g, just checking connectivity), however I could not see any response on 10g interface.
=> ping 10.137.108.231
FM1@DTSEC2 Waiting for PHY auto negotiation to complete..... TIMEOUT !
FM2@DTSEC1 Waiting for PHY auto negotiation to complete..... TIMEOUT !
FM2@DTSEC2 Waiting for PHY auto negotiation to complete..... TIMEOUT !
FM2@DTSEC3 Waiting for PHY auto negotiation to complete..... TIMEOUT !
FM2@DTSEC4 Waiting for PHY auto negotiation to complete..... TIMEOUT !
Using FM2@TGEC1 device
ping failed; host 10.137.108.231 is not alive
Please help me understand if I'm missing any configuration?
TIA.
ethtool fm2-10g
Settings for fm2-10g:
Supported ports: [ ]
Supported link modes:
Supports auto-negotiation: No
Advertised link modes: Not reported
Advertised auto-negotiation: No
Speed: Unknown! (10000)
Duplex: Full
Port: MII
PHYAD: 0
Transceiver: external
Auto-negotiation: on
Current message level: 0xffffffff (-1)
Link detected: yes
it uses linux generic 10G driver and it looks like it sets link status hard coded
so I do not think it is an indication.
U-Boot 2010.12-00001-g612800e (Jan 28 2011 - 22:20:46)
CPU0: P4080E, Version: 2.0, (0x82080020)
Core: E500MC, Version: 2.0, (0x80230020)
Clock Configuration:
CPU0:1199.988 MHz, CPU1:1199.988 MHz, CPU2:1199.988 MHz, CPU3:1199.988 MHz,
CPU4:1199.988 MHz, CPU5:1199.988 MHz, CPU6:1199.988 MHz, CPU7:1199.988 MHz,
CCB:599.994 MHz,
DDR:599.994 MHz (1199.988 MT/s data rate) (Asynchronous), LBC:74.999 MHz
FMAN1: 449.996 MHz
FMAN2: 449.996 MHz
PME: 299.997 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 4c580000 00000000 18185218 0000cccc
00000010: 4046400f 3c3c2000 fe800000 61000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
DRAM: Initializing....using SPD
Detected UDIMM(s)
Detected UDIMM(s)
Not enough bank(chip-select) for CS0+CS1+CS2+CS3 on controller 0, force non-interleaving!
Not enough bank(chip-select) for CS0+CS1+CS2+CS3 on controller 1, force non-interleaving!
Addess hashing enabled.
Addess hashing enabled.
DDR: 2 GiB (DDR3, 64-bit, CL=8, ECC on)
DDR Controller Interleaving Mode: cache line
Testing 0x00000000 - 0x7fffffff
Remap DDR
POST memory PASSED
FLASH: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 2048 KB enabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_ESDHC: 0
EEPROM: NXID v0
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, no link, regs @ 0xfe202000
PCIe3: Bus 01 - 01
Video: No radeon video card found!
In: serial
Out: serial
Err: serial
Net: Fman: Uploading microcode version 92.8.0.
Dtsec: PHY is Vitesse VSC8244 (fc6c2)
Fman: Uploading microcode version 92.8.0.
FM1@DTSEC2, FM2@TGEC1
Hit any key to stop autoboot: 0
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at e8020000 ...
Image Name: Linux-2.6.34.6-00001-g612800e
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 3355037 Bytes = 3.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at e9300000 ...
Image Name: uboot ext2 ramdisk rootfs
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 19443311 Bytes = 18.5 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at e8800000
Booting using the fdt blob at 0xe8800000
Uncompressing Kernel Image ... OK
Loading Ramdisk to 2ed75000, end 2ffffe6f ... OK
Loading Device Tree to 00ff3000, end 00fff444 ... OK
Using P4080 DS machine description
Memory CAM mapping: 256/256/256 Mb, residual: 1280Mb
Linux version 2.6.34.6-00001-g612800e (builder@builder-desktop) (gcc version 4.5.1 (Sourcery G++ Lite 2010.09-55) ) #1 SMP Fri Jan 28 22:25:52 CST 2011
Found initrd at 0xeed75000:0xeffffe6f
No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using lmb_alloc(0000000000200000)
No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using lmb_alloc(0000000001000000)
Qman ver:0a01,01,01
No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using lmb_alloc(0000000001000000)
Bman ver:0a02,01,00
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using lmb_alloc(0x0000000001000000)
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using lmb_alloc(0x0000000000a00000)
CPU maps initialized for 1 thread per core
bootconsole [udbg0] enabled
setup_arch: bootmem
Found FSL PCI host bridge at 0x0000000ffe200000. Firmware bus number: 0->0
PCI host bridge /pcie@ffe200000 ranges:
MEM 0x0000000c00000000..0x0000000c1fffffff -> 0x00000000e0000000
IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000
/pcie@ffe200000: PCICSRBAR @ 0xdf000000
Found FSL PCI host bridge at 0x0000000ffe202000. Firmware bus number: 0->0
PCI host bridge /pcie@ffe202000 ranges:
MEM 0x0000000c40000000..0x0000000c5fffffff -> 0x00000000e0000000
IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000
/pcie@ffe202000: PCICSRBAR @ 0xdf000000
P4080 DS board from Freescale Semiconductor
arch: exit
Zone PFN ranges:
DMA 0x00000000 -> 0x00030000
Normal empty
HighMem 0x00030000 -> 0x00080000
Movable zone start PFN for each node
early_node_map[1] active PFN ranges
0: 0x00000000 -> 0x00080000
MMU: Allocated 1088 bytes of context maps for 255 contexts
PERCPU: Embedded 9 pages/cpu @c200a000 s16276 r8192 d12396 u65536
pcpu-alloc: s16276 r8192 d12396 u65536 alloc=16*4096
pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [0] 4 [0] 5 [0] 6 [0] 7
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520192
Kernel command line: root=/dev/sda3 rw console=ttyS0,115200
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1991448k/2097152k available (6780k kernel code, 105704k reserved, 236k data, 423k bss, 252k init)
Kernel virtual memory layout:
* 0xfff67000..0xfffff000 : fixmap
* 0xffc00000..0xffe00000 : highmem PTEs
* 0xffbd8000..0xffc00000 : early ioremap
* 0xf1000000..0xffbd8000 : vmalloc & ioremap
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is enabled.
NR_IRQS:512 nr_irqs:512
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs
mpic: ISU size: 256, shift: 8, mask: ff
mpic: Initializing for 256 sources
clocksource: timebase mult[6aaaf09] shift[22] registered
Console: colour dummy device 80x25
Mount-cache hash table entries: 512
mpic: requesting IPIs...
Processor 1 found.
Processor 2 found.
Processor 3 found.
Processor 4 found.
Processor 5 found.
Processor 6 found.
Processor 7 found.
Brought up 8 CPUs
NET: Registered protocol family 16
e500 family performance monitor hardware support registered
PCI: Probing PCI hardware
pci 0000:00:00.0: ignoring class b20 (doesn't match header type 01)
pci 0000:00:00.0: PCI bridge to [bus 01-ff]
pci 0001:02:00.0: ignoring class b20 (doesn't match header type 01)
pci 0001:02:00.0: PCI bridge to [bus 03-ff]
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io 0xffbeb000-0xffbfafff]
pci 0000:00:00.0: bridge window [mem 0xc00000000-0xc1fffffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
pci 0001:02:00.0: PCI bridge to [bus 03-03]
pci 0001:02:00.0: bridge window [io 0xffbd9000-0xffbe8fff]
pci 0001:02:00.0: bridge window [mem 0xc40000000-0xc5fffffff]
pci 0001:02:00.0: bridge window [mem pref disabled]
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Bman err interrupt handler present
Bman portal at f1050000:f1056000 (0)
Bman portal initialised, cpu 0
Bman portal at f1060000:f105a000 (1)
Bman portal initialised, cpu 1
Bman portal at f1068000:f105e000 (2)
Bman portal initialised, cpu 2
Bman portal at f1070000:f1066000 (3)
Bman portal initialised, cpu 3
Bman portal at f1078000:f106e000 (4)
Bman portal initialised, cpu 4
Bman portal at f1080000:f1076000 (5)
Bman portal initialised, cpu 5
Bman portal at f1088000:f107e000 (6)
Bman portal initialised, cpu 6
Bman portal at f1090000:f1086000 (7)
Bman portal initialised, cpu 7
Bman portal at f1098000:f108e000 (-1)
Bman portal at f10a0000:f1096000 (-1)
Bman: reserved bpid 0, seeded 256 items
Qman err interrupt handler present
Qman portal at f10a8000:f109e000 (0:0,v0101)
Qman portal initialised, cpu 0
Qman portal at f10b0000:f10a6000 (1:1,v0101)
Qman portal initialised, cpu 1
Qman portal at f10b8000:f10ae000 (2:2,v0101)
Qman portal initialised, cpu 2
Qman portal at f10c0000:f10b6000 (3:3,v0101)
Qman portal initialised, cpu 3
Qman portal at f10c8000:f10be000 (4:4,v0101)
Qman portal initialised, cpu 4
Qman portal at f10d0000:f10c6000 (5:5,v0101)
Qman portal initialised, cpu 5
Qman portal at f10d8000:f10ce000 (6:6,v0101)
Qman portal initialised, cpu 6
Qman portal at f10e0000:f10d6000 (7:7,v0101)
Qman portal initialised, cpu 7
Qman portal at f10e8000:f10de000 (-1:8,v0101)
Qman portal at f10f0000:f10e6000 (-1:9,v0101)
Qman driver initialised
Switching to clocksource timebase
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 524288 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 18987k freed
Setting Freescale static PAMU/IOMMU configuration
Freescale PowerQUICC MII Bus: probed
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio0 has invalid PHY address
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio1 has invalid PHY address
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio2 has invalid PHY address
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio3 has invalid PHY address
Freescale XGMAC MDIO Bus: probed
mdio_bus mdio: /soc@ffe000000/fman@400000/mdio@f1000/p4080ds-xmdio1 has invalid PHY address
mdio_bus mdio: /soc@ffe000000/fman@400000/mdio@f1000/p4080ds-xmdio3 has invalid PHY address
Freescale P4080DS MDIO Bus: probed
Freescale P4080DS MDIO Bus: probed
audit: initializing netlink socket (disabled)
type=2000 audit(0.368:1): initialized
highmem bounce pool size: 64 pages
NTFS driver 2.1.29 [Flags: R/O].
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 1366
alg: No test for cipher_null (cipher_null-generic)
alg: No test for ecb(cipher_null) (ecb-cipher_null)
alg: No test for digest_null (digest_null-generic)
alg: No test for compress_null (compress_null-generic)
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Generic non-volatile memory driver v1.1
ePAPR hypervisor byte channel console driver
ehv-bc: no hypervisor found
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36) is a 16550A
console [ttyS0] enabled, bootconsole disabled
console [ttyS0] enabled, bootconsole disabled
serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36) is a 16550A
serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37) is a 16550A
serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37) is a 16550A
brd: module loaded
loop: module loaded
nbd: registered device at major 43
Freescale hypervisor management driver
fsl-hv: no hypervisor found
st: Version 20081215, fixed bufsize 32768, s/g segs 256
fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank
Amd/Fujitsu Extended Query Table at 0x0040
fe8000000.flash: CFI does not contain boot bank location. Assuming top.
number of CFI chips: 1
RedBoot partition parsing not available
fsl_espi ffe110000.spi: at 0xf11ba000 (irq = 53)
m25p80 spi32766.0: s25sl12801 (16384 Kbytes)
Creating 4 MTD partitions on "spi32766.0":
0x000000000000-0x000000100000 : "u-boot"
0x000000100000-0x000000600000 : "kernel"
0x000000600000-0x000000700000 : "dtb"
0x000000700000-0x000001000000 : "file system"
Fixed MDIO Bus: probed
Intel(R) PRO/1000 Network Driver - version 7.3.21-k5-NAPI
Copyright (c) 1999-2006 Intel Corporation.
e1000e: Intel(R) PRO/1000 Network Driver - 1.0.2-k2
e1000e: Copyright (c) 1999 - 2009 Intel Corporation.
cpu6/6: > WARNING (FM-PCD) [drivers/net/dpa/NetCommSw/Peripherals/FM/Pcd/fm_kg.c:1644 KgConfig]:
cpu6/6: numOfSchemes was defined 0 by user, re-defined by driver to FM_PCD_KG_NUM_OF_SCHEMES
cpu6/6:
cpu6/6: > WARNING (FM-PCD) [drivers/net/dpa/NetCommSw/Peripherals/FM/Pcd/fm_kg.c:1644 KgConfig]:
cpu6/6: numOfSchemes was defined 0 by user, re-defined by driver to FM_PCD_KG_NUM_OF_SCHEMES
cpu6/6:
Freescale FM module (Jan 28 2011:22:25:00)
cpu6/6: fsl_mac: FSL FMan MAC API based driver ()
cpu6/6: fsl_mac: ffe4e2000.ethernet: FMan dTSEC version: 0x08240101
cpu6/6: fsl_mac: ffe4e2000.ethernet: FMan MAC address: 00:04:9f:01:71:f4
cpu6/6: Applying 10G tx-ecc error workaround (FMAN11) ...
cpu6/6: done.
cpu6/6: fsl_mac: ffe5f0000.ethernet: FMan XGEC version: 0x0001032c
cpu6/6: fsl_mac: ffe5f0000.ethernet: FMan MAC address: 00:04:9f:01:71:fc
cpu6/6: fsl_dpa: FSL DPAA Ethernet driver ()
cpu6/6: fsl_dpa: ethernet.25: dpaa_eth.c:1740:dpa_bp_create() eth%d: Using private BM buffer pools
cpu6/6: Using dynamic RX QM frame queues
cpu6/6: Using dynamic TX QM frame queues
cpu6/6: fsl_dpa: ethernet.33: dpaa_eth.c:1740:dpa_bp_create() eth%d: Using private BM buffer pools
cpu6/6: Using dynamic RX QM frame queues
cpu6/6: Using dynamic TX QM frame queues
cpu6/6: fsl_oh: FSL FMan Offline Parsing port driver ()
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 44, io base 0xffe210000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: can't setup
fsl-ehci fsl-ehci.1: USB bus 2 deregistered
fsl-ehci fsl-ehci.1: init fsl-ehci.1 fail, -110
fsl-ehci: probe of fsl-ehci.1 failed with error -110
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
rtc-ds3232 1-0068: rtc core: registered ds3232 as rtc0
EDAC MC: Ver: 2.1.0 Jan 28 2011
Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software
EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe200000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 16 for PCI Err
MPC85xx_edac PCI err registered
EDAC PCI1: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe202000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 16 for PCI Err
MPC85xx_edac PCI err registered
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using DMA
caam ffe300000.crypto: device ID = 0x0a10020000000000
caam ffe300000.crypto: job rings = 4, qi = 1
alg: No test for authenc(hmac(sha1),cbc(aes)) (authenc-hmac-sha1-cbc-aes-caam)
caam ffe300000.crypto: authenc-hmac-sha1-cbc-aes-caam
alg: No test for authenc(hmac(sha256),cbc(aes)) (authenc-hmac-sha256-cbc-aes-caam)
caam ffe300000.crypto: authenc-hmac-sha256-cbc-aes-caam
alg: No test for authenc(hmac(sha1),cbc(des3_ede)) (authenc-hmac-sha1-cbc-des3_ede-caam)
caam ffe300000.crypto: authenc-hmac-sha1-cbc-des3_ede-caam
alg: No test for authenc(hmac(sha256),cbc(des3_ede)) (authenc-hmac-sha256-cbc-des3_ede-caam)
caam ffe300000.crypto: authenc-hmac-sha256-cbc-des3_ede-caam
alg: No test for authenc(hmac(sha1),cbc(des)) (authenc-hmac-sha1-cbc-des-caam)
caam ffe300000.crypto: authenc-hmac-sha1-cbc-des-caam
alg: No test for authenc(hmac(sha256),cbc(des)) (authenc-hmac-sha256-cbc-des-caam)
caam ffe300000.crypto: authenc-hmac-sha256-cbc-des-caam
fsl-pme ffe316000.pme: ver: 0x00100201
sample_db: starting pme2 sample DB initialisation
sample_db: db for pme ver 2.1 or greater
sample_db: pme2 sample DB initialised
Freescale pme2 db driver
Freescale pme2 scan driver
fsl-pme2-scan: device pme_scan registered
IPv4 over IPv4 tunneling driver
GRE over IPv4 tunneling driver
TCP cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
rtc-ds3232 1-0068: hctosys: unable to read the hardware clock
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Setting the hostname to p4080
Mounting filesystems
Starting syslogd and klogd
Running sysctl
Setting up networking on loopback device:
Warning: no IPADDR is set, please set this from the ltib
config screen, or directly in /etc/rc.d/rc.conf.
IP address setup bypassed
Starting inetd:
Starting the port mapper:
Starting the dropbear ssh server:
Starting the boa webserver:
Welcome to the LTIB Embedded Linux Environment
!!!!! WARNING !!!!!!!
The default password for the root account is: root
please change this password using the 'passwd' command
and then edit this message (/etc/issue) to remove this message
p4080 login:
--------u-boot---------
printenv
baudrate=115200
bdev=sda3
bootcmd=run flashboot
bootdelay=10
bootfile=uImage
c=ffe
consoledev=ttyS0
eth10addr=00:04:9F:01:71:FE
eth10addr=00:04:9F:01:71:FD
eth1addr=00:04:9F:01:71:F4
eth2addr=00:04:9F:01:71:F5
eth3addr=00:04:9F:01:71:F6
eth4addr=00:04:9F:01:71:F7
eth5addr=00:04:9F:01:71:F8
eth6addr=00:04:9F:01:71:F9
eth7addr=00:04:9F:01:71:FA
eth8addr=00:04:9F:01:71:FB
eth9addr=00:04:9F:01:71:FC
ethact=FM1@DTSEC2
ethaddr=00:04:9F:01:71:F3
fdtaddr=c00000
fdtfile=p4080ds/p4080ds.dtb
fileaddr=100000
filesize=319CB8
flashboot=setenv bootargs root=/dev/sda3 rw console=ttyS0,115200 ; bootm e8020000 e9300000 e8800000
fman_ucode=0xFEF000000ULL
gatewayip=192.168.100.0
hwconfig=fsl_ddr:addr_hash=true,ctlr_intlv=cacheline,bank_intlv=cs0_cs1_cs2_cs3
ipaddr=192.168.100.250
loadaddr=1000000
netdev=eth0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtadr
norbootaddr=e8020000
nordtbaddr=e8800000
norramdiskaddr=e9300000
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=2000000
ramdiskfile=p4080ds/rootfs.ext2.gz.uboot
remoteboot=setenv bootargs root=/dev/sda3 rw console=ttyS0,115200 ; bootm 1000000 e9300000 e8800000
rootpath=/opt/nfsroot
serverip=192.168.100.22
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $fe
uboot=u-boot.bin
ubootaddr=0xeff80000
Environment size: 1920/8188 bytes
Ok now I am using the last SDK but yet no link ;
U-Boot 2011.09 (Sep 12 2012 - 19:44:26) | ||
CPU0: P4080E, Version: 2.0, (0x82080020) | ||
Core: E500MC, Version: 2.0, (0x80230020) | ||
Clock Configuration: | ||
CPU0:1199.988 MHz, CPU1:1199.988 MHz, CPU2:1199.988 MHz, CPU3:1199.988 MHz, | ||
CPU4:1199.988 MHz, CPU5:1199.988 MHz, CPU6:1199.988 MHz, CPU7:1199.988 MHz, | ||
CCB:599.994 MHz, | ||
DDR:599.994 MHz (1199.988 MT/s data rate) (Asynchronous), LBC:74.999 MHz | ||
FMAN1: 449.996 MHz | ||
FMAN2: 449.996 MHz | ||
PME: 299.997 MHz | ||
L1: | D-cache 32 kB enabled | |
I-cache 32 kB enabled | ||
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0 | ||
36-bit Addressing | ||
Reset Configuration Word (RCW): | ||
00000000: 4c580000 00000000 18185218 0000cccc | ||
00000010: 4046400f 3c3c2000 fe800000 61000000 | ||
00000020: 00000000 00000000 00000000 008b6000 | ||
00000030: 00000000 00000000 00000000 00000000 | ||
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz | ||
I2C: ready | ||
SPI: ready | ||
DRAM: Initializing....using SPD | ||
Detected UDIMM HMT125U7BFR8C-H9 | ||
Detected UDIMM HMT125U7BFR8C-H9 | ||
CS2 is disabled. | ||
CS3 is disabled. | ||
Address hashing enabled. | ||
CS2 is disabled. | ||
CS3 is disabled. | ||
Address hashing enabled. | ||
2 GiB left unmapped | ||
4 GiB (DDR3, 64-bit, CL=8, ECC on) | ||
DDR Controller Interleaving Mode: cache line | ||
DDR Chip-Select Interleaving Mode: CS0+CS1 | ||
Testing 0x00000000 - 0x7fffffff | ||
Testing 0x80000000 - 0xffffffff | ||
Remap DDR 2 GiB left unmapped | ||
POST memory PASSED | ||
Flash: 128 MiB | ||
L2: | 128 KB enabled | |
Corenet Platform Cache: 2048 KB enabled | ||
SRIO1: disabled | ||
SRIO2: disabled | ||
MMC: FSL_ESDHC: 0 | ||
EEPROM: NXID v0 | ||
PCIe1: Root Complex, no link, regs @ 0xfe200000 | ||
PCIe1: Bus 00 - 00 | ||
PCIe2: disabled | ||
PCIe3: Root Complex, no link, regs @ 0xfe202000 | ||
PCIe3: Bus 01 - 01 | ||
In: | serial | |
Out: serial | ||
Err: serial | ||
Net: Fman1: Uploading microcode version 106.2.0 | ||
Fman2: Uploading microcode version 106.2.0 | ||
FM1@DTSEC2, FM2@TGEC1 | ||
Hit any key to stop autoboot: 0 | ||
WARNING: adjusting available memory to 30000000 | ||
## Booting kernel from Legacy Image at e8020000 ... | ||
Image Name: Linux-3.0.34-rt55-02404-g1a39570 | ||
Image Type: PowerPC Linux Kernel Image (gzip compressed) | ||
Data Size: | 3699391 Bytes = 3.5 MiB | |
Load Address: 00000000 | ||
Entry Point: 00000000 | ||
Verifying Checksum ... OK | ||
## Loading init Ramdisk from Legacy Image at e9300000 ... | ||
Image Name: fsl-image-minimal-p4080ds-201209 | ||
Image Type: PowerPC Linux RAMDisk Image (gzip compressed) | ||
Data Size: | 4694844 Bytes = 4.5 MiB | |
Load Address: 00000000 | ||
Entry Point: 00000000 | ||
Verifying Checksum ... OK | ||
## Flattened Device Tree blob at e8800000 | ||
Booting using the fdt blob at 0xe8800000 | ||
Uncompressing Kernel Image ... OK | ||
Loading Ramdisk to 2fb85000, end 2ffff33c ... OK | ||
Loading Device Tree to 03fe1000, end 03fffc05 ... OK | ||
Using P4080 DS machine description | ||
Memory CAM mapping: 256/256/256 Mb, residual: 3328Mb | ||
Linux version 3.0.34-rt55-02404-g1a39570 (leonid@Leonid2) (gcc version 4.6.2 (GCC) ) #1 SMP Sun Sep 23 11:53:52 IST 2012 | ||
Found initrd at 0xefb85000:0xeffff33c | ||
No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(0000000000200000) | ||
No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(0000000001000000) | ||
Qman ver:0a01,01,01 | ||
No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(0000000001000000) | ||
Bman ver:0a02,01,00 | ||
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using memblock_alloc(0x0000000001000000) | ||
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using memblock_alloc(0x0000000000a00000) | ||
No USDPAA memory, no 'usdpaa_mem' bootarg | ||
CPU maps initialized for 1 thread per core | ||
bootconsole [udbg0] enabled | ||
setup_arch: bootmem | ||
Found FSL PCI host bridge at 0x0000000ffe200000. Firmware bus number: 0->0 | ||
PCI host bridge /pcie@ffe200000 (primary) ranges: | ||
MEM 0x0000000c00000000..0x0000000c1fffffff -> 0x00000000e0000000 | ||
IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000 | ||
/pcie@ffe200000: PCICSRBAR @ 0xdf000000 | ||
/pcie@ffe200000: Setup 64-bit PCI DMA window | ||
/pcie@ffe200000: DMA window size is 0xdf000000 | ||
Found FSL PCI host bridge at 0x0000000ffe202000. Firmware bus number: 0->0 | ||
PCI host bridge /pcie@ffe202000 ranges: | ||
MEM 0x0000000c40000000..0x0000000c5fffffff -> 0x00000000e0000000 | ||
IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000 | ||
/pcie@ffe202000: PCICSRBAR @ 0xdf000000 | ||
/pcie@ffe202000: Setup 64-bit PCI DMA window | ||
/pcie@ffe202000: DMA window size is 0xdf000000 | ||
P4080 DS board from Freescale Semiconductor | ||
arch: exit | ||
Zone PFN ranges: | ||
DMA | 0x00000000 -> 0x00030000 | |
Normal empty | ||
HighMem 0x00030000 -> 0x00100000 | ||
Movable zone start PFN for each node | ||
early_node_map[1] active PFN ranges | ||
0: 0x00000000 -> 0x00100000 | ||
MMU: Allocated 1088 bytes of context maps for 255 contexts | ||
PERCPU: Embedded 10 pages/cpu @c27fa000 s18624 r8192 d14144 u40960 | ||
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1040384 | ||
Kernel command line: root=/dev/ram rw console=ttyS0,115200 | ||
PID hash table entries: 4096 (order: 2, 16384 bytes) | ||
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) | ||
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) | ||
Placing 64MB software IO TLB between c3ff2000 - c7ff2000 | ||
software IO TLB at phys 0x3ff2000 - 0x7ff2000 | ||
Memory: 4019808k/4194304k available (7296k kernel code, 174496k reserved, 220k data, 566k bss, 288k init) | ||
Kernel virtual memory layout: | ||
* 0xfff5f000..0xfffff000 : fixmap | ||
* 0xffc00000..0xffe00000 : highmem PTEs | ||
* 0xffbd8000..0xffc00000 : early ioremap | ||
* 0xf1000000..0xffbd8000 : vmalloc & ioremap | ||
Hierarchical RCU implementation. | ||
RCU debugfs-based tracing is enabled. | ||
NR_IRQS:512 nr_irqs:512 16 | ||
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs | ||
mpic: ISU size: 256, shift: 8, mask: ff | ||
mpic: Initializing for 256 sources | ||
clocksource: timebase mult[6aaaf09] shift[22] registered | ||
Console: colour dummy device 80x25 | ||
pid_max: default: 32768 minimum: 301 | ||
Mount-cache hash table entries: 512 | ||
mpic: requesting IPIs... | ||
e500 family performance monitor hardware support registered | ||
Brought up 8 CPUs | ||
xor: measuring software checksum speed | ||
8regs | : 1349.000 MB/sec | |
8regs_prefetch: 1176.000 MB/sec | ||
32regs | : 1274.000 MB/sec | |
32regs_prefetch: 1152.000 MB/sec | ||
xor: using function: 8regs (1349.000 MB/sec) | ||
NET: Registered protocol family 16 | ||
fsl-of-pamu fsl-of-pamu.0: implementing work-around for erratum A-004510 | ||
EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe200000.pcie' (INTERRUPT) | ||
MPC85xx_edac acquired irq 494 for PCI Err | ||
MPC85xx_edac PCI err registered | ||
EDAC PCI1: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe202000.pcie' (INTERRUPT) | ||
MPC85xx_edac acquired irq 492 for PCI Err | ||
MPC85xx_edac PCI err registered | ||
PCI: Probing PCI hardware | ||
pci 0000:00:00.0: ignoring class b20 (doesn't match header type 01) | ||
pci 0000:00:00.0: PCI bridge to [bus 01-ff] | ||
pci 0001:02:00.0: ignoring class b20 (doesn't match header type 01) | ||
pci 0001:02:00.0: PCI bridge to [bus 03-ff] | ||
pci 0000:00:00.0: PCI bridge to [bus 01-01] | ||
pci 0000:00:00.0: bridge window [io 0x0000-0xffff] | ||
pci 0000:00:00.0: bridge window [mem 0xc00000000-0xc1fffffff] | ||
pci 0000:00:00.0: bridge window [mem pref disabled] | ||
pci 0001:02:00.0: PCI bridge to [bus 03-03] | ||
pci 0001:02:00.0: bridge window [io 0xfffee000-0xffffdfff] | ||
pci 0001:02:00.0: bridge window [mem 0xc40000000-0xc5fffffff] | ||
pci 0001:02:00.0: bridge window [mem pref disabled] | ||
bio: create slab <bio-0> at 0 | ||
raid6: int32x1 | 250 MB/s | |
raid6: int32x2 | 404 MB/s | |
raid6: int32x4 | 534 MB/s | |
raid6: int32x8 | 360 MB/s | |
raid6: using algorithm int32x4 (534 MB/s) | ||
vgaarb: loaded | ||
SCSI subsystem initialized | ||
usbcore: registered new interface driver usbfs | ||
usbcore: registered new interface driver hub | ||
usbcore: registered new device driver usb | ||
Bman err interrupt handler present | ||
Bman portal initialised, cpu 0 | ||
Bman portal initialised, cpu 1 | ||
Bman portal initialised, cpu 2 | ||
Bman portal initialised, cpu 3 | ||
Bman portal initialised, cpu 4 | ||
Bman portal initialised, cpu 5 | ||
Bman portal initialised, cpu 6 | ||
Bman portal initialised, cpu 7 | ||
Bman portals initialised | ||
Bman: BPID allocator includes range 32:32 | ||
Qman err interrupt handler present | ||
Qman portal initialised, cpu 0 | ||
Qman portal initialised, cpu 1 | ||
Qman portal initialised, cpu 2 | ||
Qman portal initialised, cpu 3 | ||
Qman portal initialised, cpu 4 | ||
Qman portal initialised, cpu 5 | ||
Qman portal initialised, cpu 6 | ||
Qman portal initialised, cpu 7 | ||
Qman portals initialised | ||
Qman: FQID allocator includes range 256:256 | ||
Qman: CGRID allocator includes range 0:256 | ||
Qman: pool channel allocator includes range 33:15 | ||
Switching to clocksource timebase | ||
Switched to NOHz mode on CPU #5 | ||
Switched to NOHz mode on CPU #7 | ||
Switched to NOHz mode on CPU #1 | ||
Switched to NOHz mode on CPU #4 | ||
Switched to NOHz mode on CPU #0 | ||
Switched to NOHz mode on CPU #3 | ||
Switched to NOHz mode on CPU #6 | ||
Switched to NOHz mode on CPU #2 | ||
NET: Registered protocol family 2 | ||
IP route cache hash table entries: 32768 (order: 5, 131072 bytes) | ||
TCP established hash table entries: 131072 (order: 8, 1048576 bytes) | ||
TCP bind hash table entries: 65536 (order: 7, 524288 bytes) | ||
TCP: Hash tables configured (established 131072 bind 65536) | ||
TCP reno registered | ||
UDP hash table entries: 512 (order: 2, 16384 bytes) | ||
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes) | ||
NET: Registered protocol family 1 | ||
RPC: Registered named UNIX socket transport module. | ||
RPC: Registered udp transport module. | ||
RPC: Registered tcp transport module. | ||
RPC: Registered tcp NFSv4.1 backchannel transport module. | ||
Trying to unpack rootfs image as initramfs... | ||
rootfs image is not initramfs (no cpio magic); looks like an initrd | ||
Freeing initrd memory: 4588k freed | ||
Freescale PowerQUICC MII Bus: probed | ||
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio0 has invalid PHY address | ||
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio1 has invalid PHY address | ||
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio2 has invalid PHY address | ||
mdio_bus mdio@ffe4e1120: /soc@ffe000000/fman@400000/mdio@e1120/p4080ds-mdio3 has invalid PHY address | ||
Freescale XGMAC MDIO Bus: probed | ||
mdio_bus mdio: /soc@ffe000000/fman@400000/mdio@f1000/p4080ds-xmdio1 has invalid PHY address | ||
mdio_bus mdio: /soc@ffe000000/fman@400000/mdio@f1000/p4080ds-xmdio3 has invalid PHY address | ||
Freescale P4080DS MDIO Bus: probed | ||
Freescale P4080DS MDIO Bus: probed | ||
audit: initializing netlink socket (disabled) | ||
type=2000 audit(1.404:1): initialized | ||
highmem bounce pool size: 64 pages | ||
HugeTLB registered 4 MB page size, pre-allocated 0 pages | ||
HugeTLB registered 16 MB page size, pre-allocated 0 pages | ||
HugeTLB registered 64 MB page size, pre-allocated 0 pages | ||
HugeTLB registered 256 MB page size, pre-allocated 0 pages | ||
HugeTLB registered 1 GB page size, pre-allocated 0 pages | ||
NTFS driver 2.1.30 [Flags: R/O]. | ||
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc. | ||
msgmni has been set to 1204 | ||
async_tx: api initialized (async) | ||
io scheduler noop registered | ||
io scheduler deadline registered | ||
io scheduler cfq registered (default) | ||
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled | ||
serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36) is a 16550A | ||
console [ttyS0] enabled, bootconsole disabled | ||
console [ttyS0] enabled, bootconsole disabled | ||
serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36) is a 16550A | ||
serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37) is a 16550A | ||
serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37) is a 16550A | ||
ePAPR hypervisor byte channel driver | ||
Generic non-volatile memory driver v1.1 | ||
brd: module loaded | ||
loop: module loaded | ||
Freescale USDPAA process driver | ||
fsl-usdpaa: no region found | ||
st: Version 20101219, fixed bufsize 32768, s/g segs 256 | ||
fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000001 Chip ID 0x002801 | ||
Amd/Fujitsu Extended Query Table at 0x0040 | ||
Amd/Fujitsu Extended Query version 1.3. | ||
number of CFI chips: 1 | ||
m25p80 spi32766.0: s25sl12801 (16384 Kbytes) | ||
Creating 4 MTD partitions on "spi32766.0": | ||
0x000000000000-0x000000100000 : "u-boot" | ||
0x000000100000-0x000000600000 : "kernel" | ||
0x000000600000-0x000000700000 : "dtb" | ||
0x000000700000-0x000001000000 : "file system" | ||
fsl_espi ffe110000.spi: at 0xf117a000 (irq = 53) | ||
Fixed MDIO Bus: probed | ||
e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI | ||
e1000: Copyright (c) 1999-2006 Intel Corporation. | ||
e1000e: Intel(R) PRO/1000 Network Driver - 1.3.10-k2 | ||
e1000e: Copyright(c) 1999 - 2011 Intel Corporation. | ||
FMAN(0) Fifo size settings: | ||
- Total buffers available(512 - 256B/buffer) | ||
- Total throughput(1Gbps) | ||
- Max frame size(1522B) | ||
- 1G ports TX 1(12 bufs set (min: 12)) | ||
- 1G ports RX 1(460 bufs set (min: 14)) | ||
- OH-HC ports 4(6) | ||
- Shared extra buffers(16) | ||
FMAN(0) open dma settings: | ||
- Total open dma available(32) | ||
- 1G ports TX 1(14) | ||
- 1G ports RX 1(14) | ||
- OH-HC ports 4(1) | ||
- Shared extra open dma(0) | ||
FMAN(0) Tnums settings: | ||
- Total Tnums available(128) | ||
- 1G ports TX 1(59) | ||
- 1G ports RX 1(59) | ||
- OH-HC ports 4(2) | ||
- Shared extra tnums(2) | ||
FMAN(1) Fifo size settings: | ||
- Total buffers available(512 - 256B/buffer) | ||
- Total throughput(10Gbps) | ||
- Max frame size(1522B) | ||
- 10G ports TX 1(18 bufs set (min: 18)) | ||
- 10G ports RX 1(438 bufs set (min: 14)) | ||
- OH-HC ports 4(6) | ||
- Shared extra buffers(32) | ||
FMAN(1) open dma settings: | ||
- Total open dma available(32) | ||
- 10G ports TX 1(8) | ||
- 10G ports RX 1(8) | ||
- OH-HC ports 4(1) | ||
- Shared extra open dma(8) | ||
FMAN(1) Tnums settings: | ||
- Total Tnums available(128) | ||
- 10G ports TX 1(56) | ||
- 10G ports RX 1(56) | ||
- OH-HC ports 4(2) | ||
- Shared extra tnums(8) | ||
Freescale FM module (Sep 23 2012:11:45:13) | ||
Freescale FM Ports module (Sep 23 2012:11:45:17) | ||
cpu7: fsl_mac: FSL FMan MAC API based driver () | ||
cpu7: fsl_mac: ffe4e0000.ethernet: FMan dTSEC version: 0x08240101 | ||
cpu7: fsl_mac: ffe4e0000.ethernet: FMan MAC address: 00:04:9f:01:71:f3 | ||
cpu7: fsl_mac: ffe4e2000.ethernet: FMan dTSEC version: 0x08240101 | ||
cpu7: fsl_mac: ffe4e2000.ethernet: FMan MAC address: 00:04:9f:01:71:f4 | ||
cpu7/7: Applying 10G tx-ecc error workaround (10GMAC-A004) ... | ||
cpu7/7: done. | ||
cpu7: fsl_mac: ffe5f0000.ethernet: FMan XGEC version: 0x0001032c | ||
cpu7: fsl_mac: ffe5f0000.ethernet: FMan MAC address: 00:04:9f:01:71:fc | ||
cpu7: fsl_dpa: FSL DPAA Ethernet driver () | ||
cpu7: fsl_dpa: ethernet.14: Using private BM buffer pools | ||
cpu7: Using dynamic RX QM frame queues | ||
cpu7: Using dynamic TX QM frame queues | ||
TX Unit Test using FQ 274 | ||
Tested 18848/18848 packets. 0 failed | ||
cpu7: fsl_dpa: ethernet.15: Using private BM buffer pools | ||
cpu7: Using dynamic RX QM frame queues | ||
cpu7: Using dynamic TX QM frame queues | ||
cpu7: fsl_oh: FSL FMan Offline Parsing port driver () | ||
fsl-of-dma ffe100300.dma: dma channel dma-uio0-0 initialized | ||
fsl-of-dma ffe100300.dma: dma channel dma-uio0-1 initialized | ||
fsl-of-dma ffe100300.dma: dma channel dma-uio0-2 initialized | ||
fsl-of-dma ffe100300.dma: dma channel dma-uio0-3 initialized | ||
fsl-of-dma ffe101300.dma: dma channel dma-uio1-0 initialized | ||
fsl-of-dma ffe101300.dma: dma channel dma-uio1-1 initialized | ||
fsl-of-dma ffe101300.dma: dma channel dma-uio1-2 initialized | ||
fsl-of-dma ffe101300.dma: dma channel dma-uio1-3 initialized | ||
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver | ||
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver | ||
/soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode | ||
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller | ||
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1 | ||
fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000 | ||
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00 | ||
hub 1-0:1.0: USB hub found | ||
hub 1-0:1.0: 1 port detected | ||
Initializing USB Mass Storage driver... | ||
usbcore: registered new interface driver usb-storage | ||
USB Mass Storage support registered. | ||
mpc-i2c ffe118100.i2c: timeout 1000000 us | ||
rtc-ds3232 0-0068: rtc core: registered ds3232 as rtc0 | ||
mpc-i2c ffe118000.i2c: timeout 1000000 us | ||
mpc-i2c ffe119000.i2c: timeout 1000000 us | ||
mpc-i2c ffe119100.i2c: timeout 1000000 us | ||
md: raid6 personality registered for level 6 | ||
md: raid5 personality registered for level 5 | ||
md: raid4 personality registered for level 4 | ||
EDAC MC: Ver: 2.1.0 | ||
Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software | ||
EDAC MC0: Giving out device to 'MPC85xx_edac' 'mpc85xx_mc_err': DEV mpc85xx_mc_err | ||
MPC85xx_edac acquired irq 502 for MC | ||
MPC85xx_edac MC err registered | ||
EDAC MC1: Giving out device to 'MPC85xx_edac' 'mpc85xx_mc_err': DEV mpc85xx_mc_err | ||
MPC85xx_edac acquired irq 501 for MC | ||
MPC85xx_edac MC err registered | ||
sdhci: Secure Digital Host Controller Interface driver | ||
sdhci: Copyright(c) Pierre Ossman | ||
mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using DMA | ||
caam ffe300000.crypto: device ID = 0x0a10020000000000 | ||
caam ffe300000.crypto: job rings = 4, qi = 1 | ||
caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto | ||
platform ffe301000.jr: registering rng-caam | ||
USDPAA portal initialised, bman-uio-1 | ||
USDPAA portal initialised, bman-uio-0 | ||
USDPAA portal initialised, qman-uio-1 | ||
USDPAA portal initialised, qman-uio-0 | ||
USDPAA portal layer loaded | ||
fsl-pme ffe316000.pme: ver: 0x00100201 | ||
Freescale pme2 db driver | ||
Freescale pme2 scan driver | ||
fsl-pme2-scan: device pme_scan registered | ||
Freescale hypervisor management driver | ||
fsl-hv: no hypervisor found | ||
IPv4 over IPv4 tunneling driver | ||
TCP cubic registered | ||
Initializing XFRM netlink socket | ||
NET: Registered protocol family 10 | ||
IPv6 over IPv4 tunneling driver | ||
NET: Registered protocol family 17 | ||
NET: Registered protocol family 15 | ||
Registering the dns_resolver key type | ||
rtc-ds3232 0-0068: setting system clock to 2012-10-19 14:03:21 UTC (1350655401) | ||
md: Skipping autodetection of RAID arrays. (raid=autodetect will force) | ||
RAMDISK: gzip image found at block 0 | ||
VFS: Mounted root (ext2 filesystem) on device 1:0. | ||
Freeing unused kernel memory: 288k freed | ||
INIT: version 2.88 booting | ||
Starting udevudev[903]: renamed network interface eth0 to fm1-gb1 | ||
udev[911]: renamed network interface eth1 to fm2-10g | ||
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory | ||
bootlogd. | ||
Configuring network interfaces... ifup: don't seem to have all the variables for eth0/inet | ||
done. | ||
Running postinst /etc/rpm-postinsts/100... | ||
INIT: Entering runlevel: 5ostins | ||
Starting syslogd/klogd: done | ||
Stopping Bootlog daemon: bootlogd. | ||
Yocto (Built by Poky 6.0) 1.1 p4080ds ttyS0
************************
Please help
I tried Brian's RCW without success,
I also updated ramdisk, kernel, u-boot and Fman microcode
.... no link on PC phy
I have same problem, using freescale xaui ethernet 10g daughter board .
I got the interface in linux but no ping ,
some one can help?
Leonid