Is there an errata on the CPLD for the P2041RDB-PC? The power on these are not reliable. after turning on/off a few times, the power wouldn't come on again. It seemed like the machine was in a strange state until I pushed and held the power button and unplugged the power cord then the power button would work again.
I didn't observe this behavior when using the P2041RDB-PB.
Is it possible to replace the CPLD for the P2041RDB-PC with the CPLD for the P2041RDB-PB? If yes, how can I do that?
Thanks!
Here’s the uboot log for the P2041RDB-PC
** FROM P2041RDB-PC**********************************************
U-Boot 2013.01-00115-g831b30d (Jun 15 2013 - 05:53:49)
CPU0: P2041E, Version: 2.0, (0x82180120)
Core: E500MC, Version: 3.2, (0x80230032)
Clock Configuration:
CPU0:1500 MHz, CPU1:1500 MHz, CPU2:1500 MHz, CPU3:1500 MHz,
CCB:750 MHz,
DDR:666.667 MHz (1333.333 MT/s data rate) (Asynchronous), LBC:93.750 MHz
FMAN1: 583.333 MHz
QMAN: 375 MHz
PME: 375 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 12600000 00000000 241c0000 00000000
00000010: 248e40c0 c3c02000 de800000 40000000
00000020: 00000000 00000000 00000000 d0030f07
00000030: 00000000 00000000 00000000 00000000
Board: P2041RDB, CPLD version: 4.1 vBank: 1
SERDES Reference Clocks: Bank1=100Mhz Bank2=125Mhz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 1024 KB enabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
EEPROM: Invalid ID (ff ff ff ff)
PCIe1: disabled
PCIe2: Root Complex, x1, regs @ 0xfe201000
01:00.0 - 104c:823e - Bridge device
02:00.0 - 104c:823f - Serial bus controller
PCIe2: Bus 00 - 02
PCIe3: disabled
In: serial
Out: serial
Err: serial
Net: Initializing Fman
Fman1: DTSEC3 set to unknown interface 12
Fman1: Uploading microcode version 106.1.9
PHY reset timed out
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC4, FM1@DTSEC5, FM1@TGEC1
***************************************************************
And here’s the uboot log from P2041RDB-PB
** from P2041RDB-PB **
U-Boot 2011.12-00025-gc6d9d50 (Oct 24 2012 - 04:48:58)
CPU0: P2041E, Version: 1.1, (0x82180111)
Core: E500MC, Version: 2.2, (0x80230022)
Clock Configuration:
CPU0:1500 MHz, CPU1:1500 MHz, CPU2:1500 MHz, CPU3:1500 MHz,
CCB:750 MHz,
DDR:666.667 MHz (1333.333 MT/s data rate) (Asynchronous), LBC:93.750 MHz
FMAN1: 583.333 MHz
PME: 375 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P2041RDB, CPLD version: 4.1 vBank: 0
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 12600000 00000000 241c0000 00000000
00000010: 648ea0c1 c3c02000 de800000 40000000
00000020: 00000000 00000000 00000000 d0030f07
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100Mhz Bank2=125Mhz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM UG51U6400N8SU-ACF
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 1024 KB enabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
EEPROM: Invalid ID (ff ff ff ff)
PCIe1: disabled
PCIe2: Root Complex, x1, regs @ 0xfe201000
01:00.0 - 104c:823e - Bridge device
02:00.0 - 104c:823f - Serial bus controller
PCIe2: Bus 00 - 02
PCIe3: disabled
In: serial
Out: serial
Err: serial
Net: Initializing Fman
Fman1: Uploading microcode version 106.1.4
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5