openthread porting for NXP LS1012a

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

openthread porting for NXP LS1012a

623件の閲覧回数
sujay_g
Contributor I

Hi, I am from telecom background . I have just joined  project for openthread porting. At this point we don't have the hardware ready but the processor seems to be  NXP LS1012a . I would like to get started  porting openthread stack ,need some pointers .I found  following  link (Set Up the Build Environment  |  OpenThread )to setup build environment. 

Is there some guide available to start porting openthread to this processor ? 

0 件の賞賛
2 返答(返信)

490件の閲覧回数
sujay_g
Contributor I

Thabnks Pavel,

I have a follow up question. The openthread stack requires  board specific files , BSPs etc,

to port the stack to this platform.

 

I found following SDK . Is this the SDK to use to create the corresponding files which can be integrated to openthread stack?

there is also GitHub - qoriq-open-source/yocto-sdk    what is this used for ?

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7726177File DescriptionFile SizeFile Name
Expand All / Collapse AllCache: QorIQ Linux SDK v2.0 CORTEXA7 Yocto3.4 GBQorIQ Linux SDK v2.0 CORTEXA7 Yocto Cache.iso
0 件の賞賛

490件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following pages about OpenThread:

https://www.nxp.com/products/wireless-connectivity/proprietary-ieee-802.15.4-based/thread-networking...

 

http://events17.linuxfoundation.org/sites/events/files/slides/Building%20Multiprotocol%20IoT%20Nodes...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛