Hi,
I am looking for steps to boot ls1046 board with the yocto images, I got the kernelimage as "Image" instead of uImage/Zimage. I am trying this with NFS boot, could you help with the steps to load the images and the address.
I tried booting with
tftpboot 0x80080000 Image
tftpboot 0x90000000 Image-fsl-ls1046a-rdb.dtb
booti 0x80080000 - 0x90000000
I am getting issues
at [ 3.444391] fdt: not creating '/sys/firmware/fdt': CRC check failed
any suggestions? or manual?
已解决! 转到解答。
Look at the Section 4.4.8.9.3 of NXP SDK v2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Look at the Section 4.4.8.9.3 of NXP SDK v2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------