ls1046a emmc program uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1046a emmc program uboot

1,443 次查看
hongyuanz
Contributor IV

How to burn uboot kernel file system to emmc ..?

 

标记 (1)
0 项奖励
回复
3 回复数

1,428 次查看
hongyuanz
Contributor IV

hi yipingwang

Start via sd card root@TinyLinux:/run. . ?   program emmc

0 项奖励
回复

1,347 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Yes, starting from TinyLinux ramdisk rootfs.

0 项奖励
回复

1,436 次查看
yipingwang
NXP TechSupport
NXP TechSupport

1. Please generate atf image with RCW rcw_1600_qspiboot_emmc.rcw, and deploy ATF image on LS1046ARDB.

2. Please boot up the system with yocto tiny image, and copy flex-installer to the target board.

3. Execute the following command to deploy eMMC firmware, Linux Kernel and rootfs to eMMC card on the target board.

# ./flex-installer -i pf -p 4P=20M:1800M:20M:-1 -d /dev/mmcblk0

./flex-installer -b bootpartition_LS_arm64_lts_4.19.tgz -r rootfs_lsdk2004_ubuntu_lite_arm64.tgz -f firmware_ls1046ardb_uboot_emmcboot.img -d /dev/mmcblk0

4. Go to u-boot

=> cpld reset sd