ls1012a PFE sfp cage direct connection devicetree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1012a PFE sfp cage direct connection devicetree

1,327 Views
sergey_gavrish
Contributor II

I'm trying to connect serdes to sfp cage. Kernel config currently has option "sfp cage".

ethernet@0 {
compatible = "fsl,pfe-gemac-port";
#address-cells = <0x1>;
#size-cells = <0x0>;
reg = <0x0>;
fsl,gemac-bus-id = <0x0>;
fixed-link = <6 1 1000 0 0>;
fsl,mdio-mux-val = <0x0>;
phy-mode = "sgmii";
sfp = <0x19>;
};

sfp0 {
compatible = "sff,sfp";
i2c-bus = <0x1d>;
maximum-power-milliwatt = <0x7d0>;
phandle = <0x19>;
};

But still not work.

Can anybody help?

0 Kudos
Reply
3 Replies

1,296 Views
sergey_gavrish
Contributor II

Hi, YipingWang.

https://community.nxp.com/t5/QorIQ/SGMII-to-SFP/m-p/729582#M5863

Here your answer is: The chip does not support SGMII for backplane/PHY-less use cases.

I have more than one board for bring-up, and such dts config have success in fiber connection between two our boards, but not to network equipment with optical port. Is any way to enable SGMII in SoC as serdes media interface but not MAC interface?

 
0 Kudos
Reply

1,285 Views
yipingwang
NXP TechSupport
NXP TechSupport

The statement in LS1012A User's Manual, Section 1.4.10.3 about PHY-less SGMII being unsupported, applies _only_ to Rev.1 silicon. In that revision, you must provide a common clock between the PHY and the MAC which is not always possible in backplanes. This requirement is the impact of the chip erratum A-010336 which is fixed in Rev. 2 Summarizing, if you are going to connect LS1012A Rev.2 via a 1Gbps backplane link, you are safe to do that. Note that the recommended SerDes mode is 1000Base-KX, not SGMII. Details can be found in LS1012ARM, Section 28.7.1.3.

1000Base-KX is recommended but not mandatory. If the link partner supports auto negotiation type SGMII, PHY side, then it is OK to connect it to LS in SGMII mode. If your switch supports only the MAC side of SGMII autoneg, then you still can connect it to your  LS device, but you have to disable autoneg on the both sides. The disadvantage of this method  is that the the hardware will not setup the link automatically, it will be the task of the software.

 

0 Kudos
Reply

1,299 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try the dts definition as the following.

ethernet@0 {
compatible = "fsl,pfe-gemac-port";
#address-cells = <0x1>;
#size-cells = <0x0>;
reg = <0x0>;
fsl,gemac-bus-id = <0x0>;
fixed-link = <0 1 1000 0 0>;
fsl,mdio-mux-val = <0x0>;
phy-mode = "sgmii";
};

0 Kudos
Reply