flex-builder support for ls1043adcm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flex-builder support for ls1043adcm

958 Views
sbangalore
Contributor I

Can someone share the procedure to create a flex-builder based image for the LS1043A DCM (Dual Chip Module board)?

The procedure outlined in the DCM user manual does not use flex-builder and only shows you how to generate a Linux kernel, so it is somewhat restrictive.

Thanks in advance.

Tags (1)
0 Kudos
Reply
4 Replies

787 Views
Pavel
NXP Employee
NXP Employee

Usually u-boot provides board initialization (DDR, Flash). Look at the following pages about u-boot porting:

https://elinux.org/images/2/2a/Schulz-how-to-support-new-board-u-boot-linux.pdf

 

See also the following pages:

https://bootlin.com/pub/conferences/2015/captronic/captronic-porting-linux-on-arm.pdf

 

and

 

https://www.embedded.com/design/connectivity/4023297/Linux-Porting-Guide


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

787 Views
sbangalore
Contributor I

Thanks Pavel. This is very helpful.

0 Kudos
Reply

787 Views
sanjay_adhikari
Contributor I

I think NxP LSDK supports LS1043A-RDB. Is this LS1043A-DCM also purchased from NxP ?

0 Kudos
Reply

787 Views
sbangalore
Contributor I

Yes, this is an evaluation board from NXP containing the LS1043 and MPC5748G.

0 Kudos
Reply