evalboard for LS1043 and CPLD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

evalboard for LS1043 and CPLD

1,308 Views
trondwang
Contributor I

Hi NXP!

we have bought the evalboard for LS1043. This board has a CPLD. We have downloaded the source code for the CPLD, but it would be helpful if we had the testbench for the code. Can you provide us with the testbench?

regards Trond Wang

#ls1043a‌, CPLD

Tags (1)
0 Kudos
Reply
5 Replies

1,061 Views
trondwang
Contributor I

Hi pro-supportengineer

LS1043ARDB-PA_CPLD_V1.4.zip does not contain a testbench as far as I can see.

0 Kudos
Reply

1,061 Views
pro-supportengi
NXP Employee
NXP Employee

Does the LS1043ARDB-PA_CPLD_V1.4.zip also contain a CPLD testbench?

0 Kudos
Reply

1,061 Views
trondwang
Contributor I

Hi NXP,

the reason for asking for the testbench file is to better understand the functions of the verilog code programmed into the CPLD. The designer of the evaluation board presumably have this file.

regards Trond Wang

0 Kudos
Reply

1,061 Views
ufedor
NXP Employee
NXP Employee

The "LS1043A-RDB Rev B Design Files" package contains complete CPLD project (LS1043ARDB-PA_CPLD_V1.4.zip).

0 Kudos
Reply

1,061 Views
ufedor
NXP Employee
NXP Employee

Why you need the testbench?

Shouldn't it be requested from the CPLD manufacturer?

0 Kudos
Reply