dpl file error for LS1088

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dpl file error for LS1088

1,272 Views
ferditekce
Contributor I

Could any provide the example dpl file for LS1088a with RGMII PHY on EC1 interface?

 

Our serdis configuration is :

 

Using SERDES1 Protocol: 21 (0x15)
Using SERDES2 Protocol: 0 (0x00)

 

we have this error when apply the default dpl file or attached dpl file.

 

=> fsl_mc apply DPL 0x80300000

fsl-mc: Deploying data path layout ... WARNING: Firmware returned an error (GSR: 0x3f)

0 Kudos
3 Replies

1,102 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ferdi Tekce,

I have verified your DPL file, it was applied successfully on my LS1088ARDB board.

=> tftp 0x80300000 b25805/ls1088ardb/dpl-eth.0x15_0x00.dtb
=> fsl_mc apply DPL 0x80300000
fsl-mc: Deploying data path layout ... SUCCESS
=>

I attached MC and DPC images from LSDK 1909 release, please apply them at 0x00A00000 and 0x00E00000 on QSPI flash separately.

Thanks,

Yiping

0 Kudos

1,102 Views
ferditekce
Contributor I

Firstly, thanks for the answer! What is serdes configuration in rcw file. When I change the serdes configuration as follows, I have this error.

fsl_mc apply DPL 0x80300000

fsl-mc: Deploying data path layout ... WARNING: Firmware returned an error (GSR: 0x3f)

SERDES1 Protocol: 21 (0x15)

SERDES2 Protocol: 0 (0x00)

0 Kudos

1,102 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to serdes configuration on LS1088ARDB, please try the whether this problem remains with the following serdes configuation.

Reset Configuration Word (RCW):
       00000000: 4000541c 00000040 00000000 00000000
       00000010: 00000000 000a0000 00300000 00000000
       00000020: 034011a0 00002580 00000000 00000040
       00000030: 0000005b 00000000 00002403 00000000
       00000040: 00000000 00000000 00000000 00000000
       00000050: 00000000 00000000 00000000 00000000
       00000060: 00000000 00000000 00000011 000009e7
       00000070: 44110000 00107777
VID: Core voltage after adjustment is at 1025 mV
DRAM:  7.9 GiB
DDR    7.9 GiB (DDR4, 64-bit, CL=15, ECC on)
       DDR Chip-Select Interleaving Mode: CS0+CS1
Using SERDES1 Protocol: 29 (0x1d)
Using SERDES2 Protocol: 19 (0x13)

0 Kudos