We meets one problem when compling the u-boot using fsl toolchain for powerpc. Our puspose is to compile the uboot not using the yocoto from SDK. The following is our envirement and operation step.
1 the host is ubuntu14.04 and we installed the toolchian :fsl-qoriq-glibc-x86_64-ppc64e6500-toolchain-2.0.sh coming from SDK 2.0 and the Uboot version u-boot-2017.01.tar.bz2 (we also triend uboot 2016 version )
2 configure the board is T4240RDB_default. During the link stage , it reports the errors as the figures. It seems that the toolchain is not compatible.
3 I searched one artile in the NXP community :Cross compile U-boot with standalone tool chain from QorIQ sdk2.0 - NXP Community It suggested compiling the uboot using 32bit toolchain. So I try it according to the steps
a) install fsl-qoriq-glibc-x86_64-ppce6500-toolchain-2.0.sh and config the env
You have to use Ubuntu 14 for SDK 2.0(You are good here),
Use the t4240rdb machine in the SDK and toolchain for this machine.
Use recommended command sequence for u-boot building:
$ bitbake -c cleansstate u-boot
$ bitbake -c patch u-boot
$ bitbake -c compile -f u-boot
$ bitbake u-boot
The steps are documented in the SDK2.0 manual, Ch 3.3.1, Customizing U-Boot.
Please refer to the community post below: