We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

990 次查看
kamalakannanr
Contributor I

We are looking a Single Board computer Processor with features of 4 port PCIe x4, two Gbit ethernet port and two Rs-422 port for our product development. Please suggest if any NXP processor which supports these features

0 项奖励
回复
5 回复数

932 次查看
ufedor
NXP Employee
NXP Employee

> 4 port PCIe x4

This is a strong condition.

Only following processors/development boards are capable to support this configuration:

T2080 / T2080QDS

T4240 / T4240QDS

LS2085A

0 项奖励
回复

932 次查看
kamalakannanr
Contributor I

Will T2080 / T2080QDS T4240 / T4240QDS LS2085A support three Sensor or Video input ?

Along with 4 PCIe we want three Sensor or Video input . If any processor has this features please share.

0 项奖励
回复

932 次查看
ufedor
NXP Employee
NXP Employee

> Sensor or Video input

What are they?

0 项奖励
回复

932 次查看
kamalakannanr
Contributor I

Video input like DVI/HDMI, LVDS, ARINC 818-2 video format.

0 项奖励
回复

932 次查看
ufedor
NXP Employee
NXP Employee

Neither of the PCIe-capable processors has a video input.

0 项奖励
回复