WUSDK archive is bad?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

WUSDK archive is bad?

427 次查看
rogerdavis_mitr
Contributor I

I have downloaded the latest WUSDK file "913x_WUSDK_REL_1.3_and_p1.gz" several times and tried decompressing it on both Windows and Linux platforms using both WinZip and gzip utilities and they all indicate that the file is invalid.  Has anyone else had this problem?

#wusdk

0 项奖励
1 回复

338 次查看
Pavel
NXP Employee
NXP Employee

Calculate MD5 sum for your file.

Use the following command under Linux:

md5sum 913x_WUSDK_REL_1.3_and_p1.gz

b200642965783e9dd0c47eae05fd5c5c  913x_WUSDK_REL_1.3_and_p1.gz


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励