We are attempting to boot the TWR-LS1021A-PC Board using the prebuild images, which are already accessible on the website and the link is attached below.
But was unable to obtain the logs related to the NOR Flash. Please provide the most recent firmware image along with instructions for flashing the image into the board.
Additionally, I would like to welcome any recommendations for changes to the TWR-LS1021A-PC's build source code.
For your reference, I have attached the boot logs here.
Thanks.
Real-time edge software only provide pre-built image for SD card.
LSDK 21.08 provides firmware image for LS1021ATWR NOR flash.
$ wget https://www.nxp.com/lgfiles/sdk/lsdk2108/firmware_ls1021atwr_norboot.img
=> tftp $load_addr firmware_ls1021atwr_norboot.img
Program the composite firmware into IFC NOR flash.
• To program alternate bank:
=> protect off 64000000 +$filesize && erase 64000000 +$filesize && cp.b $load_addr 64000000 $filesize
• To program current bank:
=> protect off 60000000 +$filesize && erase 60000000 +$filesize && cp.b $load_addr 60000000 $filesize
=> run nor_bootcmd
Hi,
We have followed the suggested steps but are still unable to get the QUICC chip-related information in the boot log.
To be more specific below mentioned lines are missing from our boot log:
Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0
QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1
Kindly provide the steps to configure the source code for the QUICC module using UART.
Thanks.