Traffic accounting via pfe engine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Traffic accounting via pfe engine

655件の閲覧回数
atrifan
Contributor I

Hello,

we are trying to get per-client traffic accounting on a comcerto2k-based board which functions as a router. When the PFE engine is not enabled, we have verified that once we add iptables rules for each NAT'ed IP, we can get byte counts for these rules (the traditional way to do traffic accounting).

When enabling PFE, since the "-t nat" rules are not hit once a connection enters "fast forwarding" mode, we can not rely on the iptables counters anymore. 

Is there support in the PFE engine to provide per-IP (or per-MAC or similar) traffic accounting ? Is this something that can be implemented via pfe, or is this not supported by design ?

Thanks.

タグ(2)
0 件の賞賛
返信
1 返信

535件の閲覧回数
bpe
NXP Employee
NXP Employee

PPFE is very flexible and customizable. You requirements are good point to discuss with our ASK support team. If you have a support voucher, please don't hesitate to open a Support Case. If you don't have a voucher, consider purchasing a support plan:
http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信