We are working on T4240QDS rev 1 machine.
The current SerDes configuration that we are using is
SerDes protocol 1: 1
SerDes protocol 2: 28
SerDes protocol 3: 6
SerDes protocol 4: 12
To configure the PCI as an x8 slot we chose the values
(SRDS_PRTCL_S3 = 2 and SRDS_PRTCL_S4 = 4).
The inserted card was then booted, the kernel logs showed that the slot was still detected as a x4 slot.
Portion of the Logs:
MAC: 2, PHY: 15, SFP+: 6, PBA No: Unknown
PCI-Express bandwidth available for this card is not sufficient for optimal performance.
For optimal performance a x8 PCI-Express slot is required
How do I configure the slot (Slot 7) as a x8 slot?
已解决! 转到解答。
See the table in T4240QDSRM.pdf, your configuration SRDS_PRTCL_S4 = 4 is S4 lane ABCD for PCIe3 and EFGH for PCIe4. According to the table, this routes to SLOT7(0:3) and SLOT8(0:3)
So I think you could try the first one SD4 routes to SLOT7(0:7). To do this, Serdes protocol needs to be changed and BSM4 needs to be set (SW9[2:3]) as below.
See the table in T4240QDSRM.pdf, your configuration SRDS_PRTCL_S4 = 4 is S4 lane ABCD for PCIe3 and EFGH for PCIe4. According to the table, this routes to SLOT7(0:3) and SLOT8(0:3)
So I think you could try the first one SD4 routes to SLOT7(0:7). To do this, Serdes protocol needs to be changed and BSM4 needs to be set (SW9[2:3]) as below.