T2080 MDIC[1:0] Discrepancy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 MDIC[1:0] Discrepancy

528件の閲覧回数
neoventus
Contributor I

The T2080 reference manual states 187ohms should be used to bias the MDIO lines, while app note AN3940 states 40ohms. Can someone verify 187 is correct?

Thanks

0 件の賞賛
2 返答(返信)

447件の閲覧回数
garymilliorn
NXP Employee
NXP Employee

Also note that MDIC sets the impedance of the DDR MDQ signals, not the EMI MDIO (I know that's not what you meant).

0 件の賞賛

447件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

In case of any discrepancy between device data sheet and any other document, please trust device datasheet.

In this case, AN3940 is common appnote for devices with DDR3 controller starting from MPC85xx (note - this appnote is not listed at T2080 documentation page), whereas T2080 device datasheet contains MDIC values specific for this particular processor.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛