T1042NXE7MQB - when configured w/ four PCIe ports, do all need to use the same PLL input, i.e. PLL1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042NXE7MQB - when configured w/ four PCIe ports, do all need to use the same PLL input, i.e. PLL1?

471 Views
bradfordsmith
Contributor I

Using the T1042, I must communicate w/ 4 PCIe endpoints. All four are x1 PCIe ports, but 2 of them use a 125MHz REFCLK and the other 2 use a 100MHz REFCLK. It appears that this cannot be done with this device, that is, it appears that PCIe ports always use PLL1.

Labels (1)
0 Kudos
1 Reply

343 Views
ufedor
NXP Employee
NXP Employee

> it appears that PCIe ports always use PLL1.

Correct.

0 Kudos