T1040 L2 Switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T1040 L2 Switch

跳至解决方案
1,205 次查看
vsv
Contributor III

We have a requirement to build a switch solution for which we are considering to leverage on the L2 switch core available in T1040 processor.

The customer has asked for support of around 12-14 ports in a switch. Since the initial PoC is going to be developed with T1040RDB that has 8 ports available outside, we are planning to recommend the customer to have two RDB boards cascaded one over the other.

If we connect the 8 ports available in the RDB with end systems (server class machines, desktop PC's etc.), can we use one out of the remaining 3 ports that is available in addition, to cascade to the second switch - in which we can connect the remaining end systems.

Will this sort of topology work in making an end system connected to Switch 1 communicate with an end system connected to Switch 2?

We intend to have the end systems connected within the switch to have their communication done by the L2 switch core whereas the end systems connected to these two different switches get communicated over the T1040 processor outside the L2 Switch core?

Thanks in advance

标记 (2)
1 解答
952 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, this configuration is possible.

在原帖中查看解决方案

1 回复
953 次查看
alexander_yakov
NXP Employee
NXP Employee

Yes, this configuration is possible.