Set eSDHC polarity: P2010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set eSDHC polarity: P2010

594 Views
kajetanbrzuszcz
Contributor I

Hello, I am confused during writing driver for eSDHC for processor PowerPc P2010. In data shit there exists GUTS_PORDEVSR2 register where we can check polarity of eSDHC called SDHC_CD_
POL_SEL. But I cannot find how I can set polarity in this processor.

And also... inBooting from on-chip ROM on an MPC8536DS datasheet there exists Tip

The polarity of the SDHC_CD signal should be active-low


Anyone have some knowledge about that? 

Thanks, for your answers.

0 Kudos
Reply
1 Reply

501 Views
ufedor
NXP Employee
NXP Employee

Detailed description is provided in the AN4261 - P2020 QorIQ Integrated Processor Design Checklist, Table 27. Ethernet Pin Recommendations, TSEC2_TXD[05]/TSEC3_TX_EN:

"TSEC2_TXD[05] is a POR configuration pin for eSDHC card-detect (cfg_sdhc_cd_pol_sel) and also has an alternate function as TSEC3_TX_EN. When eTSEC1 or eTSEC2 or eTSEC3 are used as parallel interfaces, pins TSECx_TX_EN requires an external 4.7-k pull-down resistor to prevent PHY from seeing a valid Transmit Enable before it is actively driven. However, the pull-down resistor on TSEC3_TX_EN cause the eSDHC card-detect (cfg_sdhc_cd_pol_sel) to be inverted, the inversion should be overridden from the SDHCDCR [CD_INV] debug control register.
If the chip is configured to boot from eSDHC interface, SDHC_CD should be inverted on the board."

The SDHCDCR is described in the P2020 QorIQ Integrated Processor Reference Manual, 21.4.22 SDHC debug control register (GUTS_SDHCDCR).

0 Kudos
Reply