QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso i

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso i

2,575 Views
tonymoseby
Contributor II

HI,

Anyone knows where I can download " QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso"  from? I can not find it?

//T

0 Kudos
Reply
4 Replies

1,786 Views
ashish_kumar
Contributor II

you an download the from the link

https://nxp.flexnetoperations.com/control/frse/download?element=7726177 

Thanks & Regards
Satish G

0 Kudos
Reply

1,786 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Tony, 

you may get the file from this location:

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SDK_ENABLEMENT 

Regards,

0 Kudos
Reply

1,786 Views
huyho
Contributor III

Ok, I got it, I found that name after mounting iso file.

Thank you jorgeplascencia‌!

Huy.

0 Kudos
Reply

1,786 Views
huyho
Contributor III

Please give me more detail. I have the same problem.

A lot of packages, I could not find any package with name QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso!

Thank you very much!

0 Kudos
Reply