Problems with accessing PHYs on T1042D4RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with accessing PHYs on T1042D4RDB

ソリューションへジャンプ
582件の閲覧回数
arnoreinshagen
Contributor I

Hi,
I'm working with the T1042D4RDB evaluation board with the original configuration (SRDS_PRTCL_S1: 0x86).
According to the board reference manual, the 5 PHYs are attached to EMI1 with PHY_ADDR 0x01..0x05.
My question now is: through which registers in the CCSR the PHYs on EMI1 are accessible?
I tried MDIO_CTL and MDIO_DATA on all 5 EMACs, using Clause 22, but I got no response by any PHY. However, the bit MDIO_RD_ER is not set.
Can anyone give me a hint?

Kind regards,
Arno

タグ(2)
0 件の賞賛
返信
1 解決策
471件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

 

The T1042 FMan has dedicated MDIO control for external PHY management accessible at FMan MDIO address space (0xF_C000). The T1040 reference manual rev.1 mentions that, see f.e. note 2 on page 1728.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
472件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

 

The T1042 FMan has dedicated MDIO control for external PHY management accessible at FMan MDIO address space (0xF_C000). The T1040 reference manual rev.1 mentions that, see f.e. note 2 on page 1728.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信