Porting QNX on the T1042 platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting QNX on the T1042 platform

Jump to solution
696 Views
surendradhobale
Contributor III

Hello,

            I am working on the T1042 QorIQ processor. We have developed Custom board with Linux OS on it.

Currently, we have one requirement to port the QNX (QNX 6.3 and  QNX 6.5 ) on the same board.

Can we port QNX on T1042 platform?

Any supporting documents  and help from the NXP?

Thanks for the help !!!

Regards,

Surendra

Tags (3)
0 Kudos
1 Solution
507 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, QNX is proprietary OS ans supported solely by it vendor - QNX Software Systems (www.qnx.com)

There is no support for QNX available from NXP. Please contact QNX vendor for porting guide.


Have a great day,
Alexander
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
508 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry, QNX is proprietary OS ans supported solely by it vendor - QNX Software Systems (www.qnx.com)

There is no support for QNX available from NXP. Please contact QNX vendor for porting guide.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos