DDR3 DQ Signal Swapping on P1015

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 DQ Signal Swapping on P1015

696 Views
arunp
Contributor II

Can we swap the DDR3 DQ pins on the processor (P1015) side with in the byte lane, in any random fashion.

Like 

Before       After (Swapping)        DDR3 Memeory - ICSide

DQ0                 --> DQ6                    --> DDR3 D0

DQ1                 --> DQ4                    --> DDR3 D1 

DQ2                 --> DQ7                    --> DDR3 D2

DQ3                 --> DQ1                    --> DDR3 D3

DQ4                 --> DQ5                    --> DDR3 D4

DQ5                 --> DQ0                    --> DDR3 D5

DQ6                 --> DQ2                    --> DDR3 D6

DQ7                 --> DQ3                    --> DDR3 D7

The DQS and DM lines remains same.

Regards,

Arun P

0 Kudos
Reply
1 Reply

451 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Yes you can swap the DDR3 DQ pins on the processor (P1015) side within the byte lane. NXP application note “Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces” recommends ”  Pin-swap within a given byte lane to optimize the data bus routes”.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------