P4080 cache issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P4080 cache issues

1,259 次查看
JFernandes
Contributor I

Shouldn't a spinlock act as a system-wide memory barrier? I took the example given with CodeWarrior (<Install folder>/PA/CodeWarrior_Examples/Bareboard_Examples/P4080_SMP) and enabled caching. I modified the code and it's now like this:

 

extern char            *ret_from_spin_loop;
#define MASTER_CORE_ID        0
#define MAX_NUM_OF_CORES    8
unsigned long long volatile spin_table[MAX_NUM_OF_CORES] = {0x1, 0x1, 0x1, 0x1, 0x1, 0x1, 0x1, 0x1};
uint32_t spin_table_lock = 1; /* yes, locked */

 

void __spin_table_loop(void)
{
    /* I translated the original assembly code to C */
    unsigned long proc_id;
    asm ("mfpir %0" : "=r" (proc_id));
    proc_id >>= 5;
    unsigned long long TEA = 0x1;
    lwe_spin_lock(&spin_table_lock);
    do {
        TEA = spin_table[proc_id];
    } while (TEA == 0x1);
    lwe_spin_unlock(&spin_table_lock);
    
    void (*fptr)(void) = (void*)(size_t) TEA;
    fptr();
}

void __init_smp(void)
{
    unsigned long proc_id;
    asm ("mfpir %0" : "=r" (proc_id));
    proc_id >>= 5;
    if (proc_id == MASTER_CORE_ID) {
        const unsigned long startAddr = (unsigned long) &ret_from_spin_loop;
        for (int coreId = 0; coreId < MAX_NUM_OF_CORES; coreId++) {
            spin_table[coreId] = startAddr;
        }
        lwe_spin_unlock(&spin_table_lock);
    }
}

 

It happens that cores > 0 never see what core 0 writes in the spin_table array, and, consequently, never step-out of the__spin_table_loop function. What's wrong with my code?

标记 (1)
0 项奖励
回复
1 回复

1,015 次查看
TomE
Specialist II

> and enabled caching

 

Each core has its own I and D and L2 cache.

 

Are your spinlocks in shared-and-uncached memory? If not, how are you making sure all cores are seeing all accesses? What's the memory access architecture on this chip - do they snoop?

 

Tom

 

0 项奖励
回复