Hi,
Our development board using p2020 needs to support 4G SDRAM. So we need CONFIG_36BIT enable.
In board.cfg, we add our config like
Status, Arch, CPU:SPLCPU, SoC, Vendor, Board name, Target, Options,
Active powerpc mpc85xx - freescale develop-1 DEVELOP-1 -
Active powerpc mpc85xx - freescale develop-1 DEVELOP-1_36BIT develop-1:36BIT
Q1: we have a develop-1.h under include/configs/ and folder develop-1 under board/freescale/. As I know the options format <board>:[other options], so I setting develop-1:36BIT. Is it correct??
Q2: we add DEVELOP-1 first and then DEVELOP-1_36BIT. If we want to build DEVELOP-1_36BIT, should we need to type from "bitbake -c cleansstate u-boot" or what command can we use to save our time build new configuration?? For example, bitbake -c clean <target>, bitbake -c cleansstate <target>, bitbake -c cleanall <target>.
At last, we using boot code not support 36BIT in our board which have a 4G SDRAM, then we see.
Not enough bank(chip-select) for CS0+CS1 on controller 0, interleaving disabled!
Detected 4 GiB of memory
This U-Boot only supports < 4G of DDR
You could rebuild it with CONFIG_PHYS_64BIT
2 GiB (DDR3, 64-bit, CL=6, ECC off)
Thanks for any response.
Best Regard,
Kuowei Hsu
Solved! Go to Solution.
Hello Kuowei Hsu,
In SDK 1.6, P2020RDB supports 36bit u-boot, please refer to the follow 36 bit memory map.
For u-boot customizing for your target, please check whether the following steps would be better.
1. Clean u-boot Cache and get u-boot source code.
$ bitbake -c cleansstate u-boot
$ bitbake -c patch u-boot
2. Go to u-boot source folder build_p2020rdb_release/tmp/work/p2020rdb-fsl-linux-gnuspe/u-boot/2014.01+fslgit-r0/git/ to modify the source file.
Please modify these files according to your target board.
include/configs/P1_P2_RDB.h
Files in board/freescale/p1_p2_rdb_pc/, for example ddr.c, law.c, tlb.c.
3. The u-boot configuration P2020RDB-PC_36BIT has already been defined in meta-fsl-ppc/conf/machine/p2020rdb.conf
4. Rebuild U-Boot image
$ cd build_p2020rdb_release
$ bitbake -c compile -f u-boot
$ bitbake u-boot
If further assistance is needed, please feel free to let me know.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
We also modify p2020rdb.conf under meta-fsl-ppc/conf/machine/
Hello Kuowei Hsu,
In SDK 1.6, P2020RDB supports 36bit u-boot, please refer to the follow 36 bit memory map.
For u-boot customizing for your target, please check whether the following steps would be better.
1. Clean u-boot Cache and get u-boot source code.
$ bitbake -c cleansstate u-boot
$ bitbake -c patch u-boot
2. Go to u-boot source folder build_p2020rdb_release/tmp/work/p2020rdb-fsl-linux-gnuspe/u-boot/2014.01+fslgit-r0/git/ to modify the source file.
Please modify these files according to your target board.
include/configs/P1_P2_RDB.h
Files in board/freescale/p1_p2_rdb_pc/, for example ddr.c, law.c, tlb.c.
3. The u-boot configuration P2020RDB-PC_36BIT has already been defined in meta-fsl-ppc/conf/machine/p2020rdb.conf
4. Rebuild U-Boot image
$ cd build_p2020rdb_release
$ bitbake -c compile -f u-boot
$ bitbake u-boot
If further assistance is needed, please feel free to let me know.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yiping,
Thanks a lot! We build 36-bit version successfully by your suggestion. Thanks!
Best Regard,
Kuowei Hsu